|
|
|
|
|
|
|
|
| Did You Know |
 Create your account to get more discounts click here |
|
|
|
|
|
|
USB Sensor Technology
Welcome to the next level of Sensor System Integration: USB Sensor Solution! Where analog and digital output seamlessly integrate.
|
|
Smarter Solution
In January 2008, FUTEK Engineers began their research and development on the new USB Sensor Solution. The team had originally worked on USB technology for Sensors back in 2004 with FUTEK VCAL, a portable calibration verification platform. The advantage of offering a USB Solution was clear. Sensors with analog output could seamlessly interface with digital devices.
As the diagram below indicates, in order to build a Traditional Sensor System Platform, there are several instruments to consider. An ideal platform will include an Amplifier/Signal Conditioner with an Active Analog Filter which will require an external Power Supply. In addition, a Multi-meter (Display) and Data Storage is necessary. Traditional Sensors Systems also had some short comings including the power consumption, unwanted noise, and voltage drop out, that would occur if cable range between the Amplifier and Display instrument was too long. Even if we disregard the economic factor behind such a platform, the task of integrating these instruments all together is no simple feat.
As the second diagram illustrates, utilizing the USB Solution immediately removes the need for an Amplifier (Signal Conditioner), Analog Filter, Power Supply, and Multi-meter. The advantages, besides the cost, are the High Resolution Digital Output, an Integrated Digital Filter to reduce 50HZ/60HZ as well as high frequency noises, the ability to increase the sampling rate for high speed applications, and capability to store calibration values inside the on-board non-volatile memory (in order to apply the real-time calculation to account non-linearity) and also other configurations which are usually stored in a TEDS chip which is no longer needed.
The presence of a powerful micro-controller beside a high accuracy delta-sigma Analog to Digital Converter (ADC) not only eliminates analog circuitry (that reduces the sensitivity to environment conditions such as temperature, humidity and noise), but also introduces an intelligent digital system which is able to activate internal circuits such as shunt cal, short circuit protection, built in auto-calibration, integrated temperature sensor, sampling rate changer and etc., following the user prompt.
Further more, using the high speed, bi-directional USB link gives the user power to communicate with the sensor by PC based software and monitor/control the functionality of features such as tare, peak, valley and selectable averaging without any need to change the hardware settings manually.
Finally, by integrating the FUTEK USB Sensor Solution, the number of instruments interacting would be limited which makes the setup of such a platform much easier.
|
|
Traditional Sensor System
|
|
USB Sensor Solution
|
|
As the Multiple System diagram (see image to the right) illustrates the USB Sensor Solution feature can seamlessly integrate a multi sensor platform. No longer will there be a need for multiple instruments to make the platform work. FUTEK Engineers are able to connect up to 127 Sensors using the USB Sensor Solution on one port by utilizing multiple hubs . Furthermore, FUTEK can provide instruments (booster) so the system can be extended to operate on a 150 feet (45 meters) distance with no impact on the electronic noise. Such options are not easily available or user friendly for Sensors that are operating on analog platforms. The greatest advantage with such a system is that it provides flexibility in system control. If there is a failure point in the system it is much easier to determine where and which precise Sensor it is that has failed.
|
|
|
|
In the process of automating hydraulic or pneumatic presses for feedback control, traditionally one load cell was used even for heavy duty presses with a few million lbs. of load capacity. As illustrated in the enclosed diagram, multiple FUTEK load cells with built-in USB interface can easily be utilized. This approach not only simplifies the installation & handling, but also minimizes the total cost, eliminating the need for a customized sensor. In addition, it will allow the operator to check the uniform loading of a large platform while monitoring the output of each sensor individually. It also makes troubleshooting much easier, and the system will still be operational when any sensor is removed for repair or replacement. The FUTEK USB sensors, combined with FUTEK USB software utilized on a PC, will allow the development of a cost effective intelligent system without the use of multimeters, amplifiers, or data acquisition.
|
|
Internal Kit Solution
FUTEK understand the importance of quality. With that in mind, the USB Kit was designed completely by FUTEK Engineers at our Irvine Headquarter in Orange County (California). With a Sampling rate of 5 Hz / 10 Hz and a 16 bit Resolution, the USB Kit offers attractive features to consider instead of a Traditional Sensor System platform. Learn more about the the technical specifications behind the USB Technology.
|
FUTEK USB Software
FUTEK's USB Sensor Solution offers a free USB Software that provides the essential data for your system. Compatible with Windows 2000, XP and Vista, the USB Software displays the Peak/Valley, Tare/Gross with numerous filtering options.
|
USB External Kit Solution
|
|
|
|
USB210
|
|
Main Features
|
- USB bus powered
- Up to 1KHZ sampling rate
- Integrated Shunt Cal
- Input/Output Short Circuit Protection
- Integrated Operating Indicator (LED)
|
|
Specifications
|
- On-Chip Memory
- Industrial Temp Range
- Integrated Digital Filter
- 50HZ / 60H rejection (100dB)
- Digital Output Resolution
- 18 bits (ENOB rms) @ 10HZ sampling rate
- 16 bits (ENOB rms) @ 100HZ sampling rate
- 12 bits (ENOB rms) @ 500HZ sampling rate
- Input Type
- non amplified analog voltage (mV/V)
- Input Range
- Extended Input Range (optional)
- Integrated Temp Sensor (optional)
|
|
|