Shop FUTEK
CALL US TODAY
+1 (949) 465-0900
Applications ► Load Cell ► Automotive Touchscreen Haptic Feedback
 
    By Sensor Type
  • Load Cells
  • Torque Sensors
  • Pressure Sensors
  • Multi-Axis Sensors
    By Industry Type
  • Aerospace & Defense
  • Agricultural
  • Automation
  • Automotive
  • Manufacturing
  • Material & Endurance Testing
  • Medical & Pharmaceutical
  • Product Development & OEM
  • Robotic & System Integrators
    
Application 165

Automotive Touchscreen Haptic Feedback

  |  
Application Summary
As automotive entertainment UIs become more sophisticated, it’s become harder to control them hands free without looking directly at the screen. The lack of tactile feedback results in the user’s brain wanting to look at the screen to confirm input selection. By incorporating load cells to measure contact force, the on-board computer can confirm correct and incorrect inputs using varying vibrations, ensuring the driver that their input was correctly registered.
Products in Use
Four LSB200 Jr. Miniature S-Beam Load Cells each paired with an IDA100 Digitally Configurable Amplifier View Product Details
Load Cell - Automotive Touchscreen Haptic Feedback
How it Works
  1. An LSB200 Jr. Miniature S-Beam Load Cell is placed behind each of the touch screen bezel mount points. A bolt passes through each load cell holding both the screen and load cell in place.
  2. As the user taps the screen, the load cells measure the tap force.
  3. This force is then amplified via the IDA100 which is running off the cars 12V accessory power line.
  4. The amplified signal is sent to the entertainment systems computer which drives a vibrator motor proportionally in response to the contact force.
All FUTEK application illustrations are strictly conceptual. Please contact us with questions.
Load Cell - LSB200 - Jr. Miniature S-Beam Load Cells
LSB200
Jr. Miniature S-Beam Load Cells
Load Cell - IDA100 - Digitally Configurable Amplifier
IDA100
Digitally Configurable Amplifier
Subscribe to our e-newsletter!
10 Thomas, Irvine, CA 92618 USA
Tel: (949) 465-0900
Fax: (949) 465-0905


©1998-2016 FUTEK Advanced Sensor Technology, Inc. All rights reserved.

All other trademarks, service marks and logos used in this website are the property of their respective owners.