Shop FUTEK
CALL US TODAY
+1 (949) 465-0900
Applications ► Load Cell ► OEM Test Stand
 
    By Sensor Type
  • Load Cells
  • Torque Sensors
  • Pressure Sensors
  • Multi-Axis Sensors
    By Industry Type
  • Aerospace & Defense
  • Agricultural
  • Automation
  • Automotive
  • Manufacturing
  • Material & Endurance Testing
  • Medical & Pharmaceutical
  • Product Development & OEM
  • Robotic & System Integrators
    
Application 130

OEM Test Stand

  |  
Application Summary
In delicate application such as this, it becomes vital to perform accurate quality audits on equipment used in health-care practices. Therefore, utilizing OEM load cells to audit syringes (infusion pumps) provides medical quality inspectors with assurance that these apparatuses will perform up to code.
Products in Use
One Jr. Miniature S-Beam Load Cell (LSB200), OEM Load Cell (LSM Series), or Miniature Load Button (LLB Series) paired with Instrumentation (IAA Series, IPM650, IHH500, or USB Solutions) and SENSIT™ Test and Measurement Software. View Product Details
Load Cell - OEM Test Stand
How it Works
  1. In delicate application such as this, it becomes vital to perform accurate quality audits on equipment used in health-care practices. Therefore, utilizing OEM load cells to audit syringes (infusion pumps) provides medical quality inspectors with assurance that these apparatuses will perform up to code.
  2. Mounted to a mechanical lever, one of FUTEK's LSB200, LSM Series, or LLB Series load cells will measure the force applied to the syringe pump as it dispenses fluid. Product versatility allows for technicians to select the sensor that works best within their required test environment.
  3. Each of these measurements can be taken to a number of instruments for evaluation. They can be amplified and taken to a PLC using an IAA Series Analog Amplifier. Alternatively, they can be interpreted by either of FUTEK's digital displays, or streamed via FUTEK's USB Solutions.
  4. Executing SENSIT™ Test and Measurement Software alongside these digital displays or USB Solutions allows the quality inspector to data log these results. Furthermore, SENSIT™ enables technicians to analyze displacement vs force.
All FUTEK application illustrations are strictly conceptual. Please contact us with questions.
Load Cell - LSB200 - Jr. Miniature S-Beam Load Cell
LSB200
Jr. Miniature S-Beam Load Cell
Load Cell - LSM SERIES - OEM Load Cell
LSM SERIES
OEM Load Cell
Load Cell - LLB SERIES - Miniature Load Button
LLB SERIES
Miniature Load Button
Load Cell - IAA Series - Analog Amplifier
IAA Series
Analog Amplifier
Load Cell - USB SOLUTIONS - High Resolution USB Output Module
USB SOLUTIONS
High Resolution USB Output Module
Load Cell - IHH500 - Intelligent Digital Hand Held Display
IHH500
Intelligent Digital Hand Held Display
Subscribe to our e-newsletter!
10 Thomas, Irvine, CA 92618 USA
Tel: (949) 465-0900
Fax: (949) 465-0905


©1998-2019 FUTEK Advanced Sensor Technology, Inc. All rights reserved.

All other trademarks, service marks and logos used in this website are the property of their respective owners.