Shop FUTEK
CALL US TODAY
+1 (949) 465-0900
Applications ► Load Cell ► Waste Management Load Measurement
 
    By Sensor Type
  • Load Cells
  • Torque Sensors
  • Pressure Sensors
  • Multi-Axis Sensors
    By Industry Type
  • Aerospace & Defense
  • Agricultural
  • Automation
  • Automotive
  • Manufacturing
  • Material & Endurance Testing
  • Medical & Pharmaceutical
  • Product Development & OEM
  • Robotic & System Integrators
    
Application 128

Waste Management Load Measurement

  |  
Application Summary
Large waste management containers are intended to collect trash until they reach a specific capacity. Once that capacity is reached, disposal of the contents is necessary. Utilizing load cells helps monitor the container’s capacity increase.
Products in Use
Four customized Load plates paired within Instrumentation (IAA Series, IPM650, IHH500, USB Solutions). View Product Details
Load Cell - Waste Management Load Measurement
How it Works
  1. Industrial sized waste containers are able to hold 50 tons. Disposal of the contents only occurs once the container itself has reached its maximum capacity.
  2. Installing load cells at the base of the container monitors the increases in the capacity of the container.
  3. In this specific application scenario, four 25 ton load plates have to be mounted to the base of each leg of the container via two mounting options.
  4. The first mounting option is to mount the load button atop a load plate to a clean, level surface upon which the container will sit. The second mounting option is to mount the load button atop a load plate under each foot of the container.
  5. Through which ever loading methodology, the data collected by each load cell can be streamed through a summing junction box to a digital display or directly to a PC.
All FUTEK application illustrations are strictly conceptual. Please contact us with questions.
Load Cell - QLA105 - Custom Donut Load Cell
QLA105
Custom Donut Load Cell
Load Cell - IAA Series  - Analog Amplifier
IAA Series
Analog Amplifier
Load Cell - USB SOLUTIONS - High Resolution USB Output Module
USB SOLUTIONS
High Resolution USB Output Module
Load Cell - IHH500 - Intelligent Digital Hand Held Display
IHH500
Intelligent Digital Hand Held Display
Load Cell - IPM650 - Panel Mount Display
IPM650
Panel Mount Display