Applications keyboard_arrow_right Load Cell  |  Shark Bite Force Measurement

Load Cell - Shark Bite Force Measurement

Measuring the bite force of a shark was no easy task. But the engineers at Peacock Productions designed a test platform to accomplish this for Shark Week 2017. Their setup mounted several LTH500 donut load cells into a mold that simulated a shark's prey. When the shark bit down upon the mold, our sensors captured the force applied. Watch On-Demand as this all unfolds

How it Works
  1. Using several LTH500 Donut/Through Hole Load Cells, engineers were able to measure the applied force.

  2. This output was then summed with the IAC200 Summing Junction Box and sent to the IHH500 Digital Hand Held Display where the test engineers monitored and logged all resulting data.

Products in Use

Three LTH500 Donut/Through Hole Load Cells paired with a 4 Channel Summing Junction Box (IAC200) and a Digital Hand Held Display (IHH500)

Contact Us
All FUTEK application illustrations are strictly conceptual.
Please Contact Us with questions.

Measuring the bite force of a shark was no easy task. But the engineers at Peacock Productions designed a test platform to accomplish this for Shark Week 2017. Their setup mounted several LTH500 donut load cells into a mold that simulated a shark's prey. When the shark bit down upon the mold, our sensors captured the force applied. Watch On-Demand as this all unfolds

Shark Bite Force Measurement
FUTEK Certifications
Z540-1 ANSI Certified17025 ISO Certified9001 ISO Certified13485 ISO CertifiedU.S. Manufacturer
FUTEK Social Media
Please follow us on linked inPlease follow us on twitterPlease follow us on youtubePlease Email us for additional info
FUTEK Address
10 Thomas, Irvine,
CA 92618 USA
All other trademarks, service marks and logos used in this website are the property of their respective owners.
© 1998–2024 FUTEK Advanced Sensor Technology, Inc. All rights reserved.
Multi Axis Sensor, Force, Torqueapplications Shark-Bite-Force-Measurement