Applications keyboard_arrow_right Torque Sensor  |  Dental Handpiece Torque Auditing

Torque Sensor - Dental Handpiece Torque Auditing

When designing electric dental handpieces, it's crucial to understand the torque the motor generates to optimize the digital control laws. A sensor is needed in the design and testing phase of the product to capture torque generated over a wide range of conditions. With the data in hand, a more refined and capable handpiece can be developed.

How it Works
  1. A QTA141 Micro Reaction Torque Sensor is installed inline with the handpiece motor and its mount.

  2. The signal generated by the QTA141 is transmitted to the IHH500 Digital Hand Held Display for display.

  3. The signal can also be sent to the USB220 High-Resolution USB Solution for display and logging of data on a PC running our SENSIT software.

  4. Additionally, data logging can be performed with an IHH500 connected to a PC running SENSIT as well.

  5. Lastly, with the IDC305 Digital Controller with SPI, USB, and Analog Output, the sensor output can be captured via SPI into a microcontroller, USB and a PC running SENSIT, or via Analog Output into a PLC or DAQ.

  6. Lastly, with the IDC305 Digital Controller with SPI, USB, and Analog Output, the sensor output can be captured via SPI into a microcontroller, USB and a PC running SENSIT, or via Analog Output into a PLC or DAQ.

Products in Use

One QTA141 Micro Reaction Torque Sensor paired with Instrumentation (IHH500, USB220, IDC305)

Contact Us
All FUTEK application illustrations are strictly conceptual.
Please Contact Us with questions.

When designing electric dental handpieces, it's crucial to understand the torque the motor generates to optimize the digital control laws. A sensor is needed in the design and testing phase of the product to capture torque generated over a wide range of conditions. With the data in hand, a more refined and capable handpiece can be developed.

Dental Handpiece Torque Auditing
FUTEK Certifications
Z540-1 ANSI Certified17025 ISO Certified9001 ISO Certified13485 ISO CertifiedU.S. Manufacturer
FUTEK Social Media
Please follow us on linked inPlease follow us on twitterPlease follow us on youtubePlease Email us for additional info
FUTEK Address
10 Thomas, Irvine,
CA 92618 USA
All other trademarks, service marks and logos used in this website are the property of their respective owners.
© 1998–2024 FUTEK Advanced Sensor Technology, Inc. All rights reserved.
Multi Axis Sensor, Force, Torqueapplications Dental-Handpiece-Torque-Auditing