Shop FUTEK
CALL US TODAY
+1 (949) 465-0900
Applications ► Multi-Axis Sensor ► Reindeer Autopilot System
 
    By Sensor Type
  • Load Cells
  • Torque Sensors
  • Pressure Sensors
  • Multi-Axis Sensors
    By Industry Type
  • Aerospace & Defense
  • Agricultural
  • Automation
  • Automotive
  • Manufacturing
  • Material & Endurance Testing
  • Medical & Pharmaceutical
  • Product Development & OEM
  • Robotic & System Integrators
    
Application 708

Reindeer Autopilot System

  |  
Application Summary
It’s December 24 and Santa Claus has a busy night delivering gifts to the 1.3 billion children in the world. To meet his delivery schedule, Santa relies on high precision GPS navigation and autopilot systems to minimize travel time. Load feedback is necessary to confirm rein inputs and monitor reindeer health (even magical flying reindeer can grow exhausted). To monitor the reindeer, their harnesses are tied to a pair of FUTEK tri-axial load cells.
Products in Use
Two MTA600 Tri-Axial Load Cells paired with the IAA series amplifiers. View Product Details
Multi-Axis Sensor - Reindeer Autopilot System
How it Works
  1. Each reindeer line’s harnesses are each attached to a machined adapter mounted to a FUTEK MTA600 load cell.
  2. Dasher, Prancer, Comet and Donner are linked to the right hand side tri-axial load cell, while Dancer, Vixen, Cupid, and Blitzen are attached to the left hand side tri-axial load cell. Rudolph, of course, leads the pack and is linked to both lines.
  3. In flight, as the reigns pull on the reindeer’s harnesses, the load cells measure the thrust forces they generate in response on all three axes.
  4. The signal generated by the load cells is amplified and sent to the Sleigh Autopilot Navigation Travel Automation (SANTA) System.
  5. The SANTA system controls the reigns, makes course corrections and monitors the reindeer’s health as the sleigh travels across the sky bringing presents to all the boys and girls of the world.
All FUTEK application illustrations are strictly conceptual. Please contact us with questions.
Multi-Axis Sensor - MTA600 - Tri-Axial Load Cells
MTA600
Tri-Axial Load Cells
Multi-Axis Sensor - IAA Series - Analog Amplifiers
IAA Series
Analog Amplifiers
Subscribe to our e-newsletter!
10 Thomas, Irvine, CA 92618 USA
Tel: (949) 465-0900
Fax: (949) 465-0905


©1998-2016 FUTEK Advanced Sensor Technology, Inc. All rights reserved.

All other trademarks, service marks and logos used in this website are the property of their respective owners.