Applications keyboard_arrow_right Load Cell  |  Sailing Ship Rigging Tension

Load Cell - Sailing Ship Rigging Tension

Sailing ships of all sizes need to tune the rigging of their sails to
maximize performance in expected at sea conditions. This requires the
cables and ropes used in the rigging preloaded to a specified tension.
To measure the preload applied onto the ropes and cables, threaded in
line load cells are used.

How it Works
  1. An LCM525 Threaded In Line Load Cell mounts in line on the mast rigging.

  2. As the rigging is tightened, the IHH500 reads the LCM525’s output and displays it.

  3. This enables the sailor to see the line tension in real-time as they adjust the rigging.

  4. By incorporating a TEDS chip into the Binder© plug attached to the LCM525, a single IHH500 can be swapped between sensors without the need to program the IHH500 with the new sensor data.


Products in Use

LCM525 Threaded In Line Load Cell paired with an IHH500 Digital Hand Held Display

Contact Us
All FUTEK application illustrations are strictly conceptual.
Please Contact Us with questions.

Sailing ships of all sizes need to tune the rigging of their sails to
maximize performance in expected at sea conditions. This requires the
cables and ropes used in the rigging preloaded to a specified tension.
To measure the preload applied onto the ropes and cables, threaded in
line load cells are used.

Sailing Ship Rigging Tension
FUTEK Certifications
Z540-1 ANSI Certified17025 ISO Certified9001 ISO Certified13485 ISO CertifiedU.S. Manufacturer
FUTEK Social Media
Please follow us on linked inPlease follow us on twitterPlease follow us on youtubePlease Email us for additional info
FUTEK Address
10 Thomas, Irvine,
CA 92618 USA
All other trademarks, service marks and logos used in this website are the property of their respective owners.
© 1998–2024 FUTEK Advanced Sensor Technology, Inc. All rights reserved.
Multi Axis Sensor, Force, Torqueapplications Sailing-Ship-Rigging-Tension