Pressure Sensor Application | Pressure Sensor Applications
Since 1997, FUTEK has been in alliance with a French base company Technologies et Equipements Industriels (T.E.I.) for the development of the Pressure series. With T.E.I.'s 27-year experience and FUTEK's continuous leadership in the US market, the two companies have been able to 25 diffrent Pressure Sensor models.
Pressure Sensor Application Diagrams
 
Pressure Sensor Application 118 - Automation
Pressure sensors can be placed on the bottom of a silo or tank in order to monitor how full or empty it is by measuring & monitoring the pressure while knowing the volume & liquid density. Utilizing digital display controller, PLC, computer, or data acquisition sensor, you can measure ...
More
Automation
 
Pressure Sensor Application 119 - Hydraulic Systems
Most cranes, earthmovers and similar equipment are operated using hydraulic systems. In order to control the movement, holding, gripping or applied force, pressure sensors are utilized to monitor and provide pressure feedback to these systems. Using pressure sensors ...
More
Hydraulic Systems
 
Pressure Sensor Application 120 - Pressure Verification
Pressure sensors are used to measure pressure in fluid or gas applications. In this particular example, gas is compressed in the compressor. When the gas is let out it needs to be cooled down since compression of gas usually increases its temperature. The pressure sensor ...
More
Pressure Verification
 
Pressure Sensor Application 127 - Tank Level Measurement
FUTEK Advanced Sensor Technology, Inc. (FUTEK) has just added the PMP943 Miniature Pressure Sensor to their USB Sensor Solution Line. The new module with USB output eliminates the need for an analog amplifier, power supply, and display equipment making usage that much easier. The plug and play gives you power ...
More
Tank Level Measurement
 
Pressure Sensor Application 130 - Differential
Pressure sensors used in pressurized tank to measure the amount of fluid versus gas. These sensors can be mounted onto a silo or tank in order to monitor how full or empty it is by measuring & monitoring the pressure while knowing the volume & liquid density. Utilizing digital display controller, PLC, computer, or data acquisition sensor ...
More
Differential
 
Pressure Sensor Application - Flush Mount
Flush Mount Pressure Sensors with FDA approved O'Rings can be used in food production such as the dairy industry ...
More
Flush Mount