Torque Sensor Application | Torque Sensor Applications
The typical application of these products include measurements dynamometers, tool dulling indicator, motor quality control or conversion of rotary to reaction torque.
Torque Sensor Application Diagrams
 
Torque Sensor Application 114 - Peristaltic Pump
In the Peristaltic Pump, a stepping / stepper motor is used to create a pumping function and allow fluid to flow. A reaction torque sensor attached to the back end of the motor monitors the required torque and can relate the changes in torque to the flow rate or alarm the operator when the torque falls ...
More
Peristaltic Pump



 
Torque Sensor Application 115 - Prosthetic Limbs
Sensors and transducers have been very instrumental in the development of prosthetic devices. They allow prosthetic devices to closely mimic human limbs. In the example below, a smart/digital torque transducer in line with a stepper motor is providing torque & position feedback to an electronic feedback ...
More
Prosthetic Limbs
 
Load Cell and Torque Sensor Application 116 - Stamping
Different types of sensors / transducers can be used simultaneously in order to improve quality during manufacturing or production processes. Below, a torque sensor attached to a motor at the top of a stamping operation monitors the amount of torque being exerted in order to stamp the cap on top of the bottle ...
More
Stamping
 
Torque Sensor Application 117 - Assembly Line / Automation
Sensors / transducers are essential in many automated assembly, packaging and labeling processes. Below, a reaction torque sensor is setup with a servo motor in an automated conveyor belt assembly line to control the tension in the winding tape while providing feedback regarding alignment ...
More
Assembly Line / Automation
 
Torque Sensor Application 122 - Reaction Torque Sensor
Reaction Torque Sensors can be used in the measurement of Clutch/Motor rotary forces. In this application a Reaction Torque Sensor is bolted to the motor and to a fixed plate which then connects to a Clutch or Break. The rotating shaft goes through the Reaction Torque Sensor (but does not contact sensor) where it connects to the motor ...
More
Reaction Torque Sensor
 
Torque Sensor Application 136 - Break Torque / Peak Torque
FUTEK’s TFF Flange to Flange Torque Sensor Series utilize metal foil strain gauge technology, achieving optimum accuracy. Measurements can be made in clockwise and counter clockwise direction. In the illustrated application, FUTEK’s TFF was used to measure the break torque of an exercise machine for Johnson Health Tech. The company is ...
More
Break Torque / Peak Torque
 
Torque Sensor Application 139 - Torque Verification
FUTEK’s TDF line can be used for precision tests and measurements. In this application model, the TDF650 Square Drive to Flange Torque Sensor is being used to measure the accuracy of a Torque Wrench. The purpose of this application is to verify whether or not the amount of torque by the wrench is precise to its actual output. Because of its high accuracy ...
More
Torque Verification
 
Torque Sensor Application 141 - Motor Test Stand
FUTEK’s TRS705 is a Rotary Shaft-to-Shaft Torque Sensor with built-in Encoders. This example utilizes it in a motor test stand application. The purpose of the TRS705 in this application is to measure the load produced between the brake and the motor. The applied load should result is a smooth braking effect. FUTEK’s TRS705 is constructed with built-in ...
More
Motor Test Stand
 
Torque Sensor Application - Torque Screwdriver
The typical application of these products include measurements dynamometers, tool dulling indicator, motor quality control or conversion of rotary to reaction torque ...
More
Torque Screwdriver
 
Torque Sensor Application - Precision & Maintenance
The typical application of these products include measurements dynamometers, tool dulling indicator, motor quality control or conversion of rotary to reaction torque ...
More
Precision & Maintenance