Digital Load Cells
 
View All USB Load Cell Models        |        View All USB Torque Sensor Models        |        View All USB Pressure Sensor Models
 
USB Pedal Force Load Cell
FUTEK Advanced Sensor Technology, Inc. (FUTEK) has just added the LAU220 Pedal Force Load Cell to their USB Sensor Solution Line. The new module, with USB output, eliminates the need for an analog amplifier, power supply, and display equipment making usage that much easier. The plug and play gives you power to monitor the output of the sensor and enjoy measurement making it less affected by noise, temperature variation or power supply requirement. The USB integration also includes FUTEK’s USB Software which allows users to monitor the output of the Sensor in real time.
USB Reaction Torque Sensor
FUTEK Advanced Sensor Technology, Inc. (FUTEK) has just added the TFF Reaction Torque Sensor to their USB Sensor Solution Line. The new module with USB output eliminates the need for an analog amplifier, power supply, and display equipment making usage that much easier. The plug and play gives you power to monitor the output of the sensor and enjoy measurement without any worries about noise, temperature variation or power supply requirement. The USB integration also includes FUTEK’s USB Software which allows users to monitor the output of the Sensor in real time.
USB Donut Load Cell
FUTEK Advanced Sensor Technology, Inc. (FUTEK) is now offering its LTH300 Donut/Thru hole Load Cell with a USB Output option. The new module eliminates the need for an analog amplifier, power supply, and display equipment making usage that much easier. The plug and play gives you power to monitor the output of the sensor and enjoy measurement without any worries about noise, temperature variation or power supply requirement. The USB integration also includes FUTEK’s USB Software which allows users to monitor the output of the Sensor in real time.
USB Miniature Load Button
FUTEK Advanced Sensor Technology, Inc. (FUTEK) is now offering its LLB130 Miniature Load Button with a USB Output option. With the integration of the USB Kit, the need for amplifiers, filters, and multi-meters is eliminated. The USB output would give the LLB130 Miniature Load Button the ability to interface efficiently with a Data Storage Device (PC). Utilizing metal foil strain gauge technology, the LLB130 is available in 5 lbs to 50 lbs, with a subminiature 0.38 inch outside diameter.
USB High Capacity Load Cell
FUTEK Advanced Sensor Technology, Inc. (FUTEK) is now offering its LCA700 High Capacity Load Cell with a USB output option. Since the 4th quarter of 2008, FUTEK Engineering Labs have been offering USB Output option on select models. The LCA700 is now part of the FUTEK USB Sensor Solution series in the high capacity range. Utilizing metal foil strain gage technology, the LCA700 17-4PH Stainless Steel in 500,000 lbs to 1 million lbs, has a raised Spherical surface to lower the possibility of off center loading, and comes equipped with a handle for easy carrying.
USB Pancake Load Cell
FUTEK Advanced Sensor Technology Inc. (FUTEK) is pleased to present the improved LCF400 Pancake Load Cell. The design is now being offered with a brand new USB Digital Interface and is the newest product to be added to the FUTEK USB Sensor Solutions Product Line. Along with its USB output and metric threads capabilities, the LCF400 features structural changes and complete welding which drastically improves this models output symmetry and accuracy.
USB S-Beam Load Cell
FUTEK Advanced Sensor Technology, Inc. is pleased to present its LSB350 with a brand new USB Digital Interface. This improvement offers a USB type solution for Strain Gage Based Load Cells. FUTEK’s USB Sensor Solution provides an easy “Plug & Play” with basic software making the System Integration even simpler. The S Beam Load Cell has become an even more efficient product in the FUTEK Load Cell Series due to the USB output.
USB Pressure Sensor
FUTEK Advanced Sensor Technology, Inc is now offering its PFP350 Pressure Sensor with an USB output option. FUTEK Engineering Labs has been working on the USB technology since the 2nd quarter of 2008 as the demand for USB Output has increased. Utilizing metal foil strain gage technology, the PFP350 is made from 17-4 Stainless Steel, weighs 5.5 oz, has mV/V output as a standard and ranges from 300 – 10,000 psig. This PFP350 is designed and manufactured in USA.
USB Torque Sensor
FUTEK Advanced Sensor Technology, Inc is pleased to present its TFF400 Reaction Torque Sensor with a brand new USB Digital Interface with 16 bits resolution. With this improvement, FUTEK has once again shown their innovation by becoming one of the first Sensor manufacturers to offer a USB type solution for Strain Gage Based Torque Sensors. FUTEK’s USB Sensor Solution provides an easy “Plug & Play” with basic software making the System Integration even simpler.
USB Load Cell
FUTEK Advanced Sensor Technology, Inc is pleased to present its LSB200 S-Beam Jr. Load Cell with a brand new USB Digital Interface with 16 bits resolution. With this improvement, FUTEK has once again shown its innovation by becoming one of the first Sensor manufacturers to offer a USB type solution for Strain Gage Based Load Cells. FUTEK’s USB Sensor Solution provides an easy “Plug & Play” with basic software making the System Integration even simpler.