• Overview
  • Features
  • Lifetime Warranty
  • Accessories & Instruments
  • Applications
  • Support
LSB200 - S-Beam Jr.
        
 
 
Lifetime Warranty
 
A New Benchmark
Since its inception, customer satisfaction has always been the center of attention at FUTEK. Our customers have repeatedly reminded us how much they appreciate our sincere dedication to customer service, support and prompt follow up at every level. Establishing this Quality Culture has always been our focus here at FUTEK; creating a relationship of trust and loyalty with every customer and on every application. Companies that share our values know how important this is and how difficult it is to establish such a high benchmark. Our team knows that our customers value our approach as they have helped FUTEK turn into one of the fastest growing companies in Orange County. Therefore, our latest announcement launching a "No Risk Life Time Warranty" program against manufacturing defects on our popular model LSB200 Miniature S Beam Load Cell should not be a big surprise to thousands of FUTEK customers or those familiar with FUTEK culture.
 
How We Got Here
Being a Sensor Solution Source for over 20 years in demanding markets such as Medical, Aerospace and Nuclear has helped FUTEK achieve the highest level of national and international quality standard. Through these experiences we have organically created an innovative and creative team. Our engineers believe total quality starts from the design stage. Our certified technicians recognize the magnitude of their responsibilities and take complete ownership. Our technical support specialists believe in continuous education and training. Our facility is equipped with state-of-the-art technology from machining and fabrication to manufacturing and inspection and is ISO 9001:2000 certified through "DNV". Our calibration Laboratory is well equipped and certified to ISO17025 accredited by A2LA for load, Torque and pressure. In addition to all of these standards, ORACLE business suite is utilized for ultimate communication and connection from Sales to Cash while providing the impeccable traceability from start to finish.
 
A Dynamic Solution
It was extremely challenging to design multiple cryogenic sensors to meet MIT's, Jet Propulsion Labs, and NASA's space program requirements. The team spent months overcoming the multiple challenges in designing a sensor capable of monitoring the forces exerted by the drill of a Mars Robot under Martian atmospheric conditions and not fail. Our team was pushed to the edge when we had to design a sensor for a subsea torque system using a custom submersible torque sensor. The team almost gave up when we were asked to build a sensor to monitor the liquid separation forces in space but did not. In all of these cases and many more, the team was asked to accomplish the impossible and delivered every time.
 
What Sets it Apart
For us to offer our "No Risk Life Time Warranty" we accounted for all these variables and experiences to ensure our customers complete satisfaction. To initiate this program, we have selected one of our most innovative and popular products, Model LSB200 Miniature S-beam Jr. Load Cell. Starting at a capacity range of 10 grams it goes up to 100 lbs in the same 0.75" package making it ideal for environments where space is limited. With over 10,000 units sold, this model has a very impressive and spotless record in customer satisfaction. The LSB200 design features Overload Protection and is available with USB output for true plug and play applications. Starting September 1st, 2009, we will begin offering our new "No Risk Life Time Warranty" to all our customers on this model. Now there is one more reason to select and implement this remarkable product for your application.
 
Warranty Forever
FUTEK offers a Risk Free Lifetime Warranty covering all manufacturing defects for all Standard and In Stock LSB200 S-Beam Jr. Sensor products sold beginning September 1, 2009 to all customers globally.

For further peace of mind, FUTEK offers a 1 year period for customers to return units should it fail to meet the project requirements with the option of a replacement unit or a full refund. Naturally, the parts need to be in good condition for returns.

There are no exclusions on this warranty as long as your LSB200 is ordered from stock and is considered a standard product. Any modifications or custom changes made to the model, cover, or cable would be considered a non-standard product.

FUTEK is not liable for any collateral or consequential damages resulting from the use of our sensors, whether they are operating properly or not. FUTEK's sole liability shall be the value of the sensor which will be covered under normal warranty policies. “Manufacturing Defects” excludes failures resulting from customer misuse of the sensors, overloading, physical damage and abuse as determined by FUTEK's evaluation of the returned sensor. FUTEK may exercise this warranty by replacing or repairing the covered sensors, at its option on manufacturing defects. This warranty is not applicable to Instruments, Services or Accessories.