|
|
LSB Series
FUTEK’s S-Beam Load Cells offer a compact design for a variety of applications in numerous industries. Known for its high accuracy, compact design features, overload protection (in selective models), and wide capacity range, the LSB Series is a great resource of industries in need of In-Line endurance testing. These load cells are robustly constructed in the USA in either aluminum or stainless steel from 10 grams up to 25,000 lbs. capacities.
|
Overload Protection
The robust design of this LSB Series allows for the assurance of overload protection. In the instance at additional load is added during the mounting stage of the application, the LSB load cells will still function as intended. However, be cautious as to not apply any side load to this In-Line Series.
|
Capacity Range
Unique to the LSB Series is its broad capacity range. With measurements read at 10 grams to 25,000 lbs., this line has the ability to fit many applications requiring endurance testing. When pairing the USB Solutions Kit with the LSB Series, measurements can be read as small as 0.10 grams.
|
Miniature Measurements
Unique to FUTEK is the LSB200 Miniature S-Beam Jr. This small load cell has both the precision and strength to fit In-Line endurance applications. Constructed in both stainless steel and aluminum, the Miniature S-Beam Jr. is built to measure capacities of 10 grams to 100 lbs. with the added bonus of overload protection.
|
|
|