FUTEK’s Miniature Load Cells and Sub Miniature Load Cell series provide diverse solutions for Aerospace, Medical, Automotive, and Manufacturing industries. These products offer solutions for applications in both Tension and Compression. Even with the miniature design an impressive capacity range of 10 gram up to 20,000 lbs is available. In addition to our Miniature Load Cell products, FUTEK also provides Miniature Pressure, Torque and Force Sensors.
 Miniature Don’t judge the sensor by its miniature size. FUTEK’s mini sensors are strong and capable of extreme capacities in relation to its small size. These Miniature Sensors can measure a range of capacities from grams to pounds. Our Miniature S-Beam Jr. LSB200 Load Cell for example is capable of up to 0.001 g resolution using the 10 g sensor with our USB210 kit.
|
 High Endurance FUTEK’s miniature sensor line is made with the highest quality. Products within the miniature sensor solution line have been tested and gone through continuous cycles lasting up to 1.5 million cycles. FUTEK’s fatigue rated miniature sensors can last up to 10 million cycles.
|
 Intricate These tiny sensors are made by FUTEK’s highly qualified Engineering Team with trusted quality and precision. With capabilities such as (FEA) and Precision Machining, the miniature designs are pushed to the extreme. Most designs are one piece construction offering a very robust design.
|
 Overload Protection A series of FUTEK’s miniature sensor line comes with a protective feature that limits the output of the sensor protecting it from being damaged. This feature will allow you to put a capacity onto the sensor higher than the sensor’s capacity range protecting it from wear and tear. The Miniature S-Beam LSB200 Load Cell for example comes with overload protection of up to 1000% of rated output.
|
 Submersible For applications involving liquid, FUTEK sensors can also come with Submersible capabilities. These miniature sensors are submersible in any non conductive and non corrosive type liquid. From humid environments to cryogenic liquids, these sensors can withstand the most enduring environments.
|
 Watch The Video FUTEK is pleased to offer the first Miniature Digitall Load Cell with USB output and Micro Gram Part Per Million resolution. The development of this capability had many market segments in mind. The Test and Measurement industry, Nanotechnology, Pharmaceuticals, Medical Device manufacturers, Process Control of fine powder or packaging, and Aeronautical experiments.
|