Shop FUTEK
CALL US TODAY
+1 (949) 465-0900
 
FUTEK News Room
FUTEK Offers Load Cell with No Risk Life Time Warranty
Release Date: 9/14/09

A NEW BENCHMARK
FUTEK is announcing the launch of our new “No Risk Life Time Warranty” program starting September 1, 2009. Starting this month FUTEK will be offering a Life Time Warranty with our most sought out sensor, the LSB200 Miniature S-beam Load Cell on orders made on or after September 1st from stock. With the implementation of this Warranty program, we aim to extend our gratitude and appreciation to our loyal customers. FUTEK has decided to introduce its Lifetime warranty on the LSB200 to show just how confident we are in the innovation and performance of this particular product. We are also confident in our engineering precision, our manufacturing and our design capabilities offered to you with the LSB200. As a sensor manufacturer, FUTEK guarantees with the No Risk Life Time Warranty that the LSB200 will survive the series of actions taken to complete the entire specing process in any application in which the unit is being used. The No Risk Lifetime Warranty allows system integrators the assurance their FUTEK sensor will outlast the entire process of a project or application. This assurance completely eliminates the product’s shelf life, enabling customer peace of mind. FUTEK’s No Risk Life Time Warranty on the LSB200 offers Reliance, Independence, and most importantly Satisfaction, making FUTEK your Sensor Solution Source.

Lifetime Warranty 

WHAT SETS IT APART
The Miniature S-Beam Load Cell has become one of the signature products in the FUTEK Load Cell Series. This product is capable of servicing numerous applications and is used industry wide. One industry the LSB200 is often used in is the Medical Industry where it has been commonly used in medical Bag weighing applications as well as automated feedback control and inline processing applications. The LSB200 offers a perfect mixture of size, accuracy and the assurance of an overload protection feature making this one of our most sought after models. With a height of only 0.75”, the LSB200 S-Beam Jr. Load Cell is also available with a brand new USB Digital Interface with 16 bits resolution. This USB interface allows an easy plug and play and eliminates the need for an analog amplifier, power supply, and display equipment making usage easy to use and much more effective. You can enjoy measurement which is less affected by noise, temperature variation or power supply requirement with the simple plug and play system. This USB integration also gives you a power to monitor the output of the sensor and includes FUTEK’s Basic Software which allows users to monitor the output of the Sensor in real time.

LIFETIME WARRANTY
FUTEK offers a Risk Free Lifetime Warranty covering all manufacturing defects for all Standard and In Stock LSB200 S-Beam Jr. Sensor products sold beginning September 1, 2009 to all customers globally. For further peace of mind, FUTEK offers a 1 year period for customers to return units should it fail to meet the project requirements with the option of a replacement unit or a full refund. Naturally, the parts need to be in good condition for returns. There are no exclusions on this warranty as long as your LSB200 is ordered from stock and is considered a standard product. Any modifications or custom changes made to the model, cover, or cable would be considered a non-standard product. FUTEK is not liable for any collateral or consequential damages resulting from the use of our sensors, whether they are operating properly or not. FUTEK's sole liability shall be the value of the sensor which will be covered under normal warranty policies. “Manufacturing Defects” excludes failures resulting from customer misuse of the sensors, overloading, physical damage and abuse as determined by FUTEK's evaluation of the returned sensor. FUTEK may exercise this warranty by replacing or repairing the covered sensors, at its option on manufacturing defects. This warranty is not applicable to Instruments, Services or Accessories.


Subscribe to our e-newsletter!
10 Thomas, Irvine, CA 92618 USA
Tel: (949) 465-0900
Fax: (949) 465-0905


©1998-2019 FUTEK Advanced Sensor Technology, Inc. All rights reserved.

All other trademarks, service marks and logos used in this website are the property of their respective owners.