Upon power up, the TEDS enabled IPM500 will display a sequence of "3333", "2222", and "1111" followed by firmware revision
, alerting the user of TEDS capability. Ensure that the proper connections are made from pins 5 and 6 of the TEDS connector to the DB-9 converter
PCB (see Section 4) before plugging in a TEDS enabled sensor. Once the sensor is cnnected, the IPM500 will display the maufacturer's ID, and TEDS
template number followed by an automatic reset. IF the sensor contains IPM500 analog output or decimal point settings, then the display will automatically
configure these settings.
Settings
The following menu selections must be enterd before retrieving TEDS information from you TEDS enabled sensor. System must be configured for 2 point
calibration before sensor is connected, otherwise analog output settings will not setup properly.
The connectors are the screw terminals that plug into the mating jack mounted on the printed circuit board. J3 is either a 6 conductor phone
plug for RS-232/RS-485 a USB type B port with 6 pin TEDS connector (shown), or a 30 pin mass termination edge connector for parallel BCD. The USB/TEDS option
also includes a PCB DB-9 converter that connects the TEDS sensor into J5.