Applications keyboard_arrow_right Pressure Sensor  |  Ghost Containment Monitoring

Pressure Sensor - Ghost Containment Monitoring

When the Ghostbusters capture a ghost in the field, it is placed in a Ghost Trap. No ghost wants to stay trapped, so they attempt to escape by exerting pressure on the trap wall. The Ghostbusters use FUTEK’s PFT510 pressure sensor to monitor pressure in the trap and adjust the containment field appropriately.


How it Works
  1. Once the Ghostbusters have locked a ghost (a Class V Full-Roaming Vapor or weaker) into place with a one or more confinement beams, they need to capture it. This is where their patented Ghost Trap comes into play.

  2. Once inside the trap, the ghost is broken down and held in place with a laser containment grid.

  3. However, no ghost wants to stay trapped for eternity, so they attempt to break free from their prison by reforming themselves.

  4. The reforming process exerts pressure on the trap walls which is measured by the PFT510 Pressure Sensor.

  5. The pressure measurement is then fed into the trap’s controller enabling it to adjust its containment field in real time.

Products in Use

One PFT510 Flush Mount Diaphragm Miniature Pressure measurement Sensor 


Contact Us
All FUTEK application illustrations are strictly conceptual.
Please Contact Us with questions.

When the Ghostbusters capture a ghost in the field, it is placed in a Ghost Trap. No ghost wants to stay trapped, so they attempt to escape by exerting pressure on the trap wall. The Ghostbusters use FUTEK’s PFT510 pressure sensor to monitor pressure in the trap and adjust the containment field appropriately.


Ghost Containment Monitoring
FUTEK Certifications
Z540-1 ANSI Certified17025 ISO Certified9001 ISO Certified13485 ISO CertifiedU.S. Manufacturer
FUTEK Social Media
Please follow us on linked inPlease follow us on twitterPlease follow us on youtubePlease Email us for additional info
FUTEK Address
10 Thomas, Irvine,
CA 92618 USA
All other trademarks, service marks and logos used in this website are the property of their respective owners.
© 1998–2023 FUTEK Advanced Sensor Technology, Inc. All rights reserved.
Multi Axis Sensor, Force, Torqueapplications Ghost-Containment-Monitoring
+
Z540-1 ANSI Certified17025 ISO Certified9001 ISO Certified13485 ISO CertifiedU.S. Manufacturer
+
Please follow us on linked inPlease follow us on twitterPlease follow us on youtubePlease Email us for additional info
+
10 Thomas, Irvine,
CA 92618 USA
All other trademarks, service marks and logos used in this website are the property of their respective owners.
© 1998–2023 FUTEK Advanced Sensor Technology, Inc. All rights reserved.