What is Haptic Simulation in Dentistry?
Haptic Technology represents an innovative approach to dental education, leveraging the principle that the sense of touch as a new way for humans and machines to communicate. It enables interaction with digital environments through tactile feedback, allowing users to feel, manipulate, and interact with virtual objects in a simulated world. This technology is particularly transformative in dentistry, where considering human factors design is key as well as the development and refinement of psychomotor skills are crucial.
How are multi-axis force sensors used in haptic simulation technology?
Multi-axis force sensors play a crucial role in supplementing haptic simulation technology. These sensors enable haptic feedback by capturing clinician-tooth interaction forces with tri-axial force feedback (Fx, Fy, and Fz) such as compression, tension, or shear along the tooth restoration interface.
Multi-axis force sensors also aid orthodontists in understanding orthodontic biomechanics through force-feedback simulation, capturing orthodontic forces like compression of the periodontal ligament on one side and tension on the other side. This detailed force analysis enhances predictability in treatment outcomes, crucial for comprehending complex interactions between orthodontic appliances (aka braces) and teeth. Integrated within orthodontic simulators, these sensors provide real-time feedback on mechanical interactions, furthering medical research on orthodontic treatment.
Why is FUTEK's MTA250 Inline 3-Axis Load Cell suitable for Haptic simulation technology?
FUTEK's MTA250 Inline 3-Axis Load Cell (aka tri axial load cell or 3 axis sensor) stands out as a sensible component for haptic simulation technology due to its precision engineering and design attributes tailored for measuring Fx, Fy, and Fz loads, especially in low-capacity applications. Its compact design is particularly advantageous for limited spaces and size constraints, common in sophisticated simulation setups. The load cell's low profile, weighing just 0.26 lb with dimensions of 2.55" in height and 1.33" in diameter, ensures it can be seamlessly integrated into various simulation platforms without compromising the design or functionality.
Moreover, the MTA250 boasts a 300% safe overload capacity, providing exceptional durability and consistent performance during intensive use. This feature is critical in haptic simulation settings, where the types of applied forces can be either continuous forces (CF), continuous interrupted forces (CIF), and intermittent forces. Additionally, its compatibility with FUTEK USB family of digital signal conditioners and amplifiers enhances its versatility, facilitating easy integration with existing systems for real-time data processing and feedback. The inclusion of a connectorized cable simplifies assembly and servicing, further underscoring the MTA250's suitability for haptic simulation technology, where efficiency and ease of maintenance are paramount.
How it Works
Multi-axis Force Sensor: FUTEK's MTA250 tri-axial inline force sensor captures the interaction forces from the clinician-tooth with tri-axial force feedback (Fx, Fy, and Fz).
Signal Conditioning: FUTEK's USB225 Pro Elite is an ideal choice for force feedback simulation, as it offers high-speed signal sampling (up to 38,400 SPS) and advanced filtering capabilities. This ensures precise capture of orthodontic forces, enabling detailed analysis on mechanical interactions on tooth interface.
Data Logging and Analysis: To record and analyze the tri-axial force feedback data, reliable data logging software is essential. FUTEK's SENSIT data logging software combined with the load cell and the signal conditioner provides a comprehensive solution for capturing, conditioning, visualizing, and interpreting the force data obtained from haptic feedback.
Contact Us
Please Contact Us with questions.
What is Haptic Simulation in Dentistry?
Haptic Technology represents an innovative approach to dental education, leveraging the principle that the sense of touch as a new way for humans and machines to communicate. It enables interaction with digital environments through tactile feedback, allowing users to feel, manipulate, and interact with virtual objects in a simulated world. This technology is particularly transformative in dentistry, where considering human factors design is key as well as the development and refinement of psychomotor skills are crucial.
How are multi-axis force sensors used in haptic simulation technology?
Multi-axis force sensors play a crucial role in supplementing haptic simulation technology. These sensors enable haptic feedback by capturing clinician-tooth interaction forces with tri-axial force feedback (Fx, Fy, and Fz) such as compression, tension, or shear along the tooth restoration interface.
Multi-axis force sensors also aid orthodontists in understanding orthodontic biomechanics through force-feedback simulation, capturing orthodontic forces like compression of the periodontal ligament on one side and tension on the other side. This detailed force analysis enhances predictability in treatment outcomes, crucial for comprehending complex interactions between orthodontic appliances (aka braces) and teeth. Integrated within orthodontic simulators, these sensors provide real-time feedback on mechanical interactions, furthering medical research on orthodontic treatment.
Why is FUTEK's MTA250 Inline 3-Axis Load Cell suitable for Haptic simulation technology?
FUTEK's MTA250 Inline 3-Axis Load Cell (aka tri axial load cell or 3 axis sensor) stands out as a sensible component for haptic simulation technology due to its precision engineering and design attributes tailored for measuring Fx, Fy, and Fz loads, especially in low-capacity applications. Its compact design is particularly advantageous for limited spaces and size constraints, common in sophisticated simulation setups. The load cell's low profile, weighing just 0.26 lb with dimensions of 2.55" in height and 1.33" in diameter, ensures it can be seamlessly integrated into various simulation platforms without compromising the design or functionality.
Moreover, the MTA250 boasts a 300% safe overload capacity, providing exceptional durability and consistent performance during intensive use. This feature is critical in haptic simulation settings, where the types of applied forces can be either continuous forces (CF), continuous interrupted forces (CIF), and intermittent forces. Additionally, its compatibility with FUTEK USB family of digital signal conditioners and amplifiers enhances its versatility, facilitating easy integration with existing systems for real-time data processing and feedback. The inclusion of a connectorized cable simplifies assembly and servicing, further underscoring the MTA250's suitability for haptic simulation technology, where efficiency and ease of maintenance are paramount.