Applications keyboard_arrow_right Load Cell  |  Medical Guidewire Test

Load Cell - Medical Guidewire Test

In the medical industry, guidewire testing can provide a means of evaluating material quality, and core wire consistency and reliability. In this automated guidewire testing system FUTEK’s LSB200 is integrated to the wire clamp, guided by an actuator, to record the peak force or breaking force of the guidewire under test.


How it Works
  1. Medical guidewire testing systems enables two types of wire tensile testing: destructive and non-destructive.

  2. During a destructive guidewire tensile test, a guidewire is secured between a prescribed clamp on one end and a clamp on the other. The guidewire is then pulled apart until the specimen breaks.

  3. During a non-destructive guidewire tensile test, a guidewire is secured between a prescribed clamp on one end and a clamp on the other. The guidewire is then pulled at a controlled rate until a specific force is reached to ensure high reliability and safety of wire.

  4. FUTEK’s LSB200 Jr. Miniature S-Beam Load Cell is attached in line with the automated clamp to measure the pulling force exerted on the guidewire under test.

  5. FUTEK's IHH500 can capture and display the peak force right before wire breakage.

Products in Use

Jr. Miniature S-Beam Load Cell (LSB200) paired with Instrumentation (IHH500 Display).


Contact Us
All FUTEK application illustrations are strictly conceptual.
Please Contact Us with questions.

In the medical industry, guidewire testing can provide a means of evaluating material quality, and core wire consistency and reliability. In this automated guidewire testing system FUTEK’s LSB200 is integrated to the wire clamp, guided by an actuator, to record the peak force or breaking force of the guidewire under test.


Medical Guidewire Test
Multi Axis Sensor, Force, Torqueapplications Medical-Guidewire-Test
+
Z540-1 ANSI Certified17025 ISO Certified9001 ISO Certified13485 ISO CertifiedU.S. Manufacturer
+
Please follow us on linked inPlease follow us on twitterPlease follow us on youtubePlease Email us for additional info
+
10 Thomas, Irvine,
CA 92618 USA
All other trademarks, service marks and logos used in this website are the property of their respective owners.
© 1998–2023 FUTEK Advanced Sensor Technology, Inc. All rights reserved.