Applications keyboard_arrow_right Torque Sensor  |  OEM Torque Motor Stand

Torque Sensor | OEM Torque Sensors | Motor Torque Stand

Reaction torque sensors are often used as auditing and monitoring tools. This application utilizes the FUTEK TFF Series (OEM torque sensors) to measure the reaction torque produced by a miniature electric DC (brushed/brushless) or AC motor using a torque sensor amplifier.

How it Works
  1. In this application, a reaction torque sensor is mounted to the electric motor with the motor shaft passing freely through the torque sensor.

  2. For optimal performance of the reaction torque sensor, the free end of the sensor, as pictured, must be fixed.

  3. The TFF Series measures the reaction torque/torsion moments created by the miniature electric motor during operation, acting as an electric motor torque sensor.

  4. These measurements are then amplified with IAA Series or IDA100 for use with PLCs and data acquisition devices or streamed to the PC with IDA100 over USB.

  5. In addition, with the IDA100, data can be viewed in real time and logged by operators using FUTEK’s SENSIT™ Test and Measurement Software.

Products in Use

One Reaction Torque Sensor (TFF Series) paired with Instrumentation (IAA  series analog amplifier or the IDA100 digitally configurable
amplifier).

Contact Us
All FUTEK application illustrations are strictly conceptual.
Please Contact Us with questions.

Reaction torque sensors are often used as auditing and monitoring tools. This application utilizes the FUTEK TFF Series (OEM torque sensors) to measure the reaction torque produced by a miniature electric DC (brushed/brushless) or AC motor using a torque sensor amplifier.

electric oem motor torque sensors torque sensor amplifier
Multi Axis Sensor, Force, Torqueapplications OEM-Torque-Motor-Stand
+
Z540-1 ANSI Certified17025 ISO Certified9001 ISO Certified13485 ISO CertifiedU.S. Manufacturer
+
Please follow us on linked inPlease follow us on twitterPlease follow us on youtubePlease Email us for additional info
+
10 Thomas, Irvine,
CA 92618 USA
All other trademarks, service marks and logos used in this website are the property of their respective owners.
© 1998–2023 FUTEK Advanced Sensor Technology, Inc. All rights reserved.