Applications keyboard_arrow_right Load Cell  |  Trailing Cone

Trailing Cone Drag Force Measurement | FUTEK

What is a Trailing Cone?

Trailing cones (aka trailing wires or trailing static cones) is a testing device used to calibrate the static pressure (i.e. altimetry ) of an aircraft. It provides accurate atmospheric pressure measurements surrounding the aircraft. To accomplish accurate measurements, the trailing cone sits clear outside of the pressure disturbance region around the aircraft fuselage or at least one fuselage length behind the aircraft and it is connected to the control system thru a pressure tubing.


During the product development phase of new aircraft, the cone is fixed on to test planes during early test flights to measure static pressure or ambient atmospheric pressure.


How to measure trailing cone drag force?

In some critical flight test validations, aeronautical engineers need to determine the aerodynamic drag forces on the cone and compare them to analytical predictions. In those instances, in-line load cells are installed in the trailing cone system to measure the axial tension in the pressure tube caused by the cone drag force.


These in-line force measurements allow flight test engineers to validate analytical models and accurately determine in-flight loads exerted on the cone attachment point.


In this application, two types of in line load cells were used to measure the tension in the tube. The first type, LCM325, is solid and prevented the pressure transducer from sensing static pressure. The second type, QLA317 is hollow and allowed the static pressure to flow through the load cell to the pressure transducer. The load cells were installed between the attachment point and the pressure tube.

How it Works
  1. A precision load cell is installed in-line with the pressure tube that connects the trailing cone and the ambient static pressure measurement system.

  2. The cone is then attached to the tip of the aircraft's vertical stabilizer (aka tail).

  3. During the flight test, the trailing cone system is dragged by the aircraft and the aerodynamic drag force is measured by the in-line load cell.

Products in Use

LCM325: Miniature Threaded In-Line Load Cell
QLA317: Custom In-Line Thru Hole Load Cell

Contact Us
All FUTEK application illustrations are strictly conceptual.
Please Contact Us with questions.

What is a Trailing Cone?

Trailing cones (aka trailing wires or trailing static cones) is a testing device used to calibrate the static pressure (i.e. altimetry ) of an aircraft. It provides accurate atmospheric pressure measurements surrounding the aircraft. To accomplish accurate measurements, the trailing cone sits clear outside of the pressure disturbance region around the aircraft fuselage or at least one fuselage length behind the aircraft and it is connected to the control system thru a pressure tubing.


During the product development phase of new aircraft, the cone is fixed on to test planes during early test flights to measure static pressure or ambient atmospheric pressure.


How to measure trailing cone drag force?

In some critical flight test validations, aeronautical engineers need to determine the aerodynamic drag forces on the cone and compare them to analytical predictions. In those instances, in-line load cells are installed in the trailing cone system to measure the axial tension in the pressure tube caused by the cone drag force.


These in-line force measurements allow flight test engineers to validate analytical models and accurately determine in-flight loads exerted on the cone attachment point.


In this application, two types of in line load cells were used to measure the tension in the tube. The first type, LCM325, is solid and prevented the pressure transducer from sensing static pressure. The second type, QLA317 is hollow and allowed the static pressure to flow through the load cell to the pressure transducer. The load cells were installed between the attachment point and the pressure tube.

trailing cone drag force
Multi Axis Sensor, Force, Torqueapplications Trailing-Cone
+
Z540-1 ANSI Certified17025 ISO Certified9001 ISO Certified13485 ISO CertifiedU.S. Manufacturer
+
Please follow us on linked inPlease follow us on twitterPlease follow us on youtubePlease Email us for additional info
+
10 Thomas, Irvine,
CA 92618 USA
All other trademarks, service marks and logos used in this website are the property of their respective owners.
© 1998–2023 FUTEK Advanced Sensor Technology, Inc. All rights reserved.