Loading...

Load Cell - UAV Launcher Force

Contact Us

Unmanned aerial vehicles (UAVs) come with a variety of launching capablities, such as hand launching, vertical takeoff, or runway takeoff. With the rise of ever more capable and powerful UAVs, some vehicles require launchers are needed to propel them into the air. These launchers need to apply a minimum amount of force to safely launch the aircraft into the air. To accomplish this, an LCB400 Rod End Load Cell is mated to the launching mechanism to measure the force applied to the UAV.


How it Works

  1. The fixed end of an LCB400 Rod End Load Cell is mounted to the end of a linear actuator.

  2. The active end of the LCB400 is then attached to the cable that will pull the UAV.

  3. The actuator piston is then rapidly retracted, pulling the cable that will launch the aircraft into the air.

  4. The LCB400 measures the force applied to the cable by the actuator.

  5. The measurement from the LCB400 is sent to the digital display (SENSLOG Handheld Display, IPM650 Panel Mount Display) or displayed on a PC with our SENSIT software (IDA100).

  6. An amplified analog signal is then sent to the PLC controlling launcher and enabling force control.

  7. Additionally, our SENSIT software can be used to log sensor output from our SENSLOG Handheld Display and IDA100.

Products in Use

One LCB400 Rod End Load Cell paired with Instrumentation (IAA Series, SENSLOG Handheld Display, IPM650 Panel Mount Display, or IDA100)


UAV Launcher Force

Contact Us

Tell us about your application and we'll connect you to a specialist.

All FUTEK application illustrations are strictly conceptual. Contact us for any questions.

(949) 465-0900

Mon-Fri, 7am - 5pm Pacific