Applications keyboard_arrow_right Torque Sensor  |  Torque Verification/Calibration

Torque Sensor - Torque Verification/Calibration (304)

Application Summary

Reaction Torque Sensors are frequently used as auditing tools. This application is utilizing FUTEK’s TDF Torque Sensor to verify the precision of a torque wrench.


Products in Use

One Reaction Torque Sensor (TDF Series) paired with Instrumentation (IPM650, IHH500 or USB Solution).


Torque Verification/Calibration
How it Works
  1. FUTEK’s TDF Series is an efficient tool to use when auditing torque wrenches.

  2. In this application, the TDF Reaction Torque Sensor is fixed to a mounting plate and coupled to a torque wrench using a male/female adapter.

  3. As the operator ratchets the torque wrench up and down, FUTEK’s TDF Sensor will measure the torque being applied.

  4. These measurements are sent directly to a paired instrument. Depending on instrument selection, the operator can either view the data on a digital display or stream the data directly onto a PC.

  5. If the data shows any anomalies, the torque wrench may be in need of recalibration to meet its intended spec.