Applications keyboard_arrow_right Load Cell  |  Catheter Force Measurement

Load Cell - Catheter Force Measurement

Accuracy and sensitivity are extremely critical during intravascular procedures. In this application, FUTEK’s LSB200 Miniature S-Beam Jr. Load Cell gives medical practitioners the force measurement accuracy and precision that is necessary for robotic intravascular procedures.




How it Works
  1. Catheter procedures demand the utmost precision and leave little margin for error.

  2. Feedback provided by the LSB200 gives physicians the necessary force measurements to navigate the catheter safely.

  3. In the above application, a Jr. Miniature S-Beam Load Cell (LSB200) is located on the guide wire extending from the robotic arm. The LSB200 measures tension on the wire and this information is used to control the  direction and motion of the catheter.

  4. Measurement feedback can be streamed through FUTEK’s USB Solutions to a central control system.

Products in Use

Jr. Miniature S-Beam Load Cell (LSB200) paired with Instrumentation (USB Solutions or IAA Series Analog Amplifier)




Contact Us
All FUTEK application illustrations are strictly conceptual.
Please Contact Us with questions.

Accuracy and sensitivity are extremely critical during intravascular procedures. In this application, FUTEK’s LSB200 Miniature S-Beam Jr. Load Cell gives medical practitioners the force measurement accuracy and precision that is necessary for robotic intravascular procedures.




Catheter Force Measurement
FUTEK Certifications
Z540-1 ANSI Certified17025 ISO Certified9001 ISO Certified13485 ISO CertifiedU.S. Manufacturer
FUTEK Social Media
Please follow us on linked inPlease follow us on twitterPlease follow us on youtubePlease Email us for additional info
FUTEK Address
10 Thomas, Irvine,
CA 92618 USA
All other trademarks, service marks and logos used in this website are the property of their respective owners.
© 1998–2024 FUTEK Advanced Sensor Technology, Inc. All rights reserved.
Multi Axis Sensor, Force, Torqueapplications Catheter-Force-Measurement