Applications keyboard_arrow_right Load Cell  |  Package Drop Test

Package Drop Test | Drop Test Packaging | Drop Test Machine

What is a Package Drop Test?

What is drop test in packaging? A package drop test is a standardized method employed to assess the robustness and protective qualities of packaging materials. It involves subjecting the package to controlled impacts, simulating the forces experienced during handling, stacking, and transportation. By understanding the behavior of the packaging under realistic conditions, engineers can optimize designs and materials, leading to improved product protection, reduced returns, and increased customer satisfaction.


The ASTM D5276 standard assesses the impact of anticipated free-falls on both the package and its contents in the context of shipping and distribution. Such free-falls may happen when a package is accidentally dropped during transit or if it undergoes rough handling throughout the distribution process.

Package Drop Test Machine Overview
Package drop test machines are specifically designed to mimic the conditions of real-world impacts. Packaging drop test machine enables precise control over the height, orientation, and impact surfaces, allowing engineers to conduct standardized drop tests. They consist of a rigid framework, a drop platform, and various measurement sensors, including load cells, to capture critical data during the test.

How load cells are used in Packaging Drop Test Machines?
To accomplish a ideal drop test environment, a system is designed to drop packages from varying heights onto a platform that rests upon load cells placed beneath the platform. The load cells output the force of the impact of the packaging. In addition, by making the platform removable, different platforms can be constructed to test different drops, such as dropping downstairs.

How it Works
  1. Four LCF series pancake load cells are mount on the four corners of the drop test machine base. The drop test packaging platform is then bolted over the four load cells.

  2. When a package is dropped, the load cells in each corner measure and send load data to the USB530 data acquisition unit.

  3. The data collected is displayed, logged, and graphed via our SENSIT™ software on a PC.

  4. By changing out the test platform, different drop scenarios can be simulated and recorded for study and compliance with testing standards such as ASTM D5276 and ISTA 1a, 2a, and 3a.

Products in Use

FUTEK’s Pancake Load Cells (LCF Series) coupled with USB530 High Speed, External USB Kit.

Contact Us
All FUTEK application illustrations are strictly conceptual.
Please Contact Us with questions.

What is a Package Drop Test?

What is drop test in packaging? A package drop test is a standardized method employed to assess the robustness and protective qualities of packaging materials. It involves subjecting the package to controlled impacts, simulating the forces experienced during handling, stacking, and transportation. By understanding the behavior of the packaging under realistic conditions, engineers can optimize designs and materials, leading to improved product protection, reduced returns, and increased customer satisfaction.


The ASTM D5276 standard assesses the impact of anticipated free-falls on both the package and its contents in the context of shipping and distribution. Such free-falls may happen when a package is accidentally dropped during transit or if it undergoes rough handling throughout the distribution process.

Package Drop Test Machine Overview
Package drop test machines are specifically designed to mimic the conditions of real-world impacts. Packaging drop test machine enables precise control over the height, orientation, and impact surfaces, allowing engineers to conduct standardized drop tests. They consist of a rigid framework, a drop platform, and various measurement sensors, including load cells, to capture critical data during the test.

How load cells are used in Packaging Drop Test Machines?
To accomplish a ideal drop test environment, a system is designed to drop packages from varying heights onto a platform that rests upon load cells placed beneath the platform. The load cells output the force of the impact of the packaging. In addition, by making the platform removable, different platforms can be constructed to test different drops, such as dropping downstairs.

package drop test drop test packaging package drop test machine what is drop test in packaging
Multi Axis Sensor, Force, Torqueapplications Package-Drop-Test