Applications keyboard_arrow_right Load Cell  |  Robotic Tactile Sensing
Application 117
Robotic Tactile Sensing
Application Summary

Multiple Load Button Load Cells are utilized to measure the tactile force produced by an industrial robot. FUTEK has developed a technical article detailing the use of load cells in robotic prosthetics and grippers.


Products in Use

Five Miniature Load Buttons (LLB Series) paired with FUTEK's USB Solutions and SENSIT™ Test and Measurement Software.


How it Works
  1. As research laboratories continue to explore the world of robotics, there exists a greater necessity for high precision test and measurement products.

  2. This application illustrates five Miniature Load Buttons mounted to the tip of each robotic finger. As the robotic hand manipulates different objects, the force require to handle those particular objects is collected.

  3. Pairing FUTEK's USB Solution with these Load Buttons, research engineers can stream the multiple force directly onto their PC.

  4. If their PC utilizes FUTEK's SENSIT™ Test and Measurement Software, the engineers will be able to live graph and log all the data.