Applications keyboard_arrow_right Load Cell  |  Tube Expansion Measurement

Load Cell - Tube Expansion Measurement

Utilizing a Load Button, engineers can measure the expansion of a tube as fluid moves through it.


How it Works
  1. FUTEK's LLB Series Miniature Load Button is installed between two plates. Also located between these plates is a process tube.

  2. As fluid flows through the process tube, its diameter expands. The unique design of this plate (pivot points), allows for this expansion to occur.

  3. As the tube expands, the top plate begins to apply force measurements onto the load button.

  4. This applied force is then streamed to one of several instrument options - a digital display, an amplifier, or a USB module.

  5. Both the digital displays as well as the USB module can utilize FUTEK's  SENSIT™ Test and Measurement Software to graph and collect the data.

Products in Use

LLB Series Miniature Load Button paired with Instrumentation (USB Solutions, IAA Series, IHH500, and IPM650).


Contact Us
All FUTEK application illustrations are strictly conceptual.
Please Contact Us with questions.

Utilizing a Load Button, engineers can measure the expansion of a tube as fluid moves through it.


Tube Expansion Measurement
FUTEK Certifications
Z540-1 ANSI Certified17025 ISO Certified9001 ISO Certified13485 ISO CertifiedU.S. Manufacturer
FUTEK Social Media
Please follow us on linked inPlease follow us on twitterPlease follow us on youtubePlease Email us for additional info
FUTEK Address
10 Thomas, Irvine,
CA 92618 USA
All other trademarks, service marks and logos used in this website are the property of their respective owners.
© 1998–2024 FUTEK Advanced Sensor Technology, Inc. All rights reserved.
Multi Axis Sensor, Force, Torqueapplications Tube-Expansion-Measurement