Applications keyboard_arrow_right Torque Sensor  |  Torque Verification/Calibration
Application 304
Torque Verification/Calibration
Application Summary

Reaction Torque Sensors are frequently used as auditing tools. This application is utilizing FUTEK’s TDF Torque Sensor to verify the precision of a torque wrench.


Products in Use

One Reaction Torque Sensor (TDF Series) paired with Instrumentation (IPM650, IHH500 or USB Solution).


How it Works
  1. FUTEK’s TDF Series is an efficient tool to use when auditing torque wrenches.

  2. In this application, the TDF Reaction Torque Sensor is fixed to a mounting plate and coupled to a torque wrench using a male/female adapter.

  3. As the operator ratchets the torque wrench up and down, FUTEK’s TDF Sensor will measure the torque being applied.

  4. These measurements are sent directly to a paired instrument. Depending on instrument selection, the operator can either view the data on a digital display or stream the data directly onto a PC.

  5. If the data shows any anomalies, the torque wrench may be in need of recalibration to meet its intended spec.