Loading...

Load Cells for Sale | FUTEK

What is a load cell and what are the different types of load cells for sale?

Get to know the functionalities and capabilities of various load cells and find various models of load cells for sale.


Force Transducer manufactured in US by FUTEK Advanced Sensor Technology (FUTEK), a leading manufacturer producing a huge selection of sensors, utilizing one of the most advanced technologies in the Sensor Industry: Metal foil strain gauge technology. A Force Transducer is defined as a sensor that converts an input mechanical load, weight, tension, compression or pressure into an electrical output signal (load cell definition). Force Measuring sensors are also commonly known as Load Sensors. There are several types of load cells based on size, geometry and capacity.


What is a Load Cell?

By definition, force sensor is a type of transducer, specifically a force transducer. It converts an input mechanical force such as load, weight, tension, compression or pressure (i.e. pressure measurement) into another physical variable, in this case, into an electrical output signal that can be measured, converted and standardized. As the force applied to the weight sensor increases, the electrical signal changes proportionally.

Transducers became an essential element in many industries from Automotive, High precision manufacturing, Aerospace & Defense, Industrial Automation, Medical & Pharmaceuticals and Robotics where reliable and high precision force measurement is paramount (i,e. medical load cell). Most recently, with the advancements in Collaborative Robots (Cobots) and Surgical Robotics, many novel force measurement applications are emerging.

 

LCM100 Miniature In Line Load Cell:

LTH300 Donut Thru Hole Load Cell - Force Washer

 

 Check out our Store. More than 600+ types of load cell transducers available!

 

How does a Load Cell work for Measuring Force?

Firstly, we need to understand the underlying physics and material science behind the force sensor working principle, which is the strain gauge (sometimes referred to as Strain gage). Metal foil strain gage is a sensor whose electrical resistance varies with applied force. In other words, it converts (or transduces) force, pressure, tension, compression, torque, weight, etc… into a change in electrical resistance, which can then be measured. 

Strain gauges are electrical conductors tightly attached to a film in a zigzag shape. When this film is pulled, it — and the conductors — stretches and elongates. When it is pushed, it is contracted and gets shorter. This change in shape causes the resistance in the electrical conductors to also change. The strain applied in the load cell can be determined based on this principle, as strain gauge resistance increases with applied strain and diminishes with contraction.

 

load cells for sale force sensor transducer strain gauge load cell
Fig 1: Metal Foil Strain gage. Source: ScienceDirect

 

Structurally, a load cell sensor is made of a metal body (also called flexure) to which foil strain gauges are bonded. The sensor body is usually made of aluminum or stainless steel, which gives the sensor two important characteristics: (1) provides the sturdiness to withstand high loads and (2) has the elasticity to minimally deform and return to its original shape when the force is removed. 

When force (tension or compression) is applied, the metal body acts as a “spring” and is slightly deformed, and unless it is overloaded, it returns to its original shape. As the flexure deforms, the strain gage also changes its shape and consequently its electrical resistance, which creates a differential voltage variation through a Wheatstone Bridge circuit. Thus, the change in voltage is proportional to the physical force applied to the flexure, which can be calculated via the load cell circuit voltage output.

Fig. 2: Strain gauge deformation in both tension and compression.

 

These strain gauges are arranged in what is called a Wheatstone Bridge Circuit (see animated diagram). This means that four strain gages are interconnected as a loop circuit (load cell circuit) and the measuring grid of the force being measured is aligned accordingly. 

The strain gauge bridge amplifiers (or load cell signal conditioners) provide regulated excitation voltage to the load cell circuit and convert the mv/V output signal into another form of signal that is more useful to the user (i.e. load cell adc). The signal generated by the strain gage bridge is low strength signal and may not work with other components of the system, such as PLC, data acquisition modules (DAQ), load cell data logger, computers, or microprocessors. Thus, strain gauge signal conditioner functions include excitation voltage, noise filtering or attenuation, signal amplification, and output signal conversion. 

Furthermore, the change in the amplifier voltage output is calibrated to be linearly proportional to the Newtonian force applied to the flexure, which can be calculated via the load cell circuit voltage equation.

 

Talk to our Application Specialists. 600+ types of sensors available!

 

Fig. 3: Strain Gauge Circuit – Full Bridge Wheatstone Circuit.

 

An important concept regarding strain gauge load cells is load cell sensitivity and accuracy. Sensor accuracy can be defined as the smallest amount of force that can be applied to the sensor body required to cause a linear and repeatable variation in the voltage output. The higher the load cell accuracy, the better, as it can consistently capture very sensible force variations. In applications like high precision factory automation, surgical robotics, aerospace, load cell linearity is paramount in order to accurately feed the PLC or DAQ control system with the accurate measurement. Some of our Universal Pancake Load Cells presents Nonlinearity of ±0.1% (of Rated Output) and Nonrepeatability of ±0.05% RO, which make them an adequate model for rocket engine thrust test stand applications.

 

What are the advantages of strain gage-based load cells?

Metal foil strain gauge force transducers are the most common technology, given its high accuracy, long term reliability, variety of shapes and sensor geometry and cost-effectiveness when compared to other measurement technologies. Also, strain gage sensors are less affected by temperature variations.

  • The highest accuracy which may conform to many standards from Surgical Robotics to Aerospace;
  • Robust Construction made of either high strength Stainless steel or Aluminum;
  • Maintain high performance at the longest possible work life even at the most rigorous conditions. Some load cell designs can go up to billions of fully reversed cycles (lifespan).
  • A plethora of geometries and customized shapes, as well as mounting options for ANY scale ANY-where.
  • A full gamut of selections with capacities ranging from 10 grams to 100,000 pounds.

 

What are the types of strain gauge-based load cell transducers?

Although there several technologies to measuring force, we will focus on the most common type of load cell: metal foil strain gauge. Within the types of force sensors, there are a variety of body shapes and geometries, each one catering to distinct applications. Get to know them if you want to buy load cell:

  • In-Line Load Cell – Most commonly referred to as in-line load cell or a canister-style (or column) sensor with male threads. This style of force sensor can be used in both tension and compression loading applications. In-line sensors offer high accuracy and high stiffness with minimal mounting clearance needed. They are great for endurance, press in force measurement applications and in instances where a micro force sensor (aka miniature force sensor, mini load cell or micro load cell) is required.
  • Load Button – These force transducers have a single flat, raised surface (aka a button) where the compressive force is applied. What’s impressive about load buttons is their low profile load cell design. As small load cells as they are, they are known for their robustness and are used in fatigue applications. Rolling element bearing load measurement is an application where load buttons are utilized.
  • S-Beam Load Cell – With other names including Shear Beam Load Cell or S-Type load transducers, the S-Beam force sensor is a compression load cell and tension load cell sensors with female threads for mounting. Sporting high accuracy and a thin beam load cell, compact profile, this sensor type is great for in-line processing and automated control feedback applications. S Beam Load cells can also be used as a non contact flow sensor in fluid flow measurement application.
  • Thru-Hole Load Cell – Also known as donut load cell or washer load cell, thru-hole load cell traditionally have a smooth non-threaded inner diameter used to measure compressive loads that require a rod to pass through its center. One of the primary uses of this sensor type is to measure bolt loading.
  • Pancake Load Cells – Pancake, canister-style, or universal load cells have a central threaded hole for measuring loads in either tension or compression. These sensors are used in applications needing high endurance, high fatigue life, or high-capacity in-line measurements such as material force testing applications and load cell for tanks weighing system. They are also highly resistant to off-axis loading are also available as low profile pancake load cell.
  • Rod-End Load Cell – Also known as Actuator Load Cell, this load transducer type offers one male thread and one female thread for mounting. The male and female thread combination is well suited in applications where you need to adapt a sensor into an existing fixture.
  • Bending Beam Load Cell - Offers a slim design making it ideal for OEM applications. Utilized in Compression, the Bending Beam Load Cells can be used to measure force, surface pressure and displacement for OEM Applications. With its miniature size, the Cantilever Load Cell is a great selection for tight environments.
  • Single Point Load Cell -  Side mounted load cell with a single point design that are specifically made for OEM applications that require high precision or high volume production. These strain gauged based force sensors measure tension and compression and are also known as compact parallelogram sensors, or single point load cell. Side mount load cells such as the LSM300 model are a recommended OEM weight measurement solution for automatic bottle filling machines.

Other unique designs are also available such as the load pin load cells (aka load cell pin), seat belt load cell, and others. 

 

 
LLB130 Subminiature Load Cells Load Button
 
LCA305 Miniature Column Load Cell

  

Speak to our Force Sensor Specialists. 600+ types of load cells available!

 

How to choose a load cell for your application?

We understand that choosing the right load transducer is a daunting task, as there is no real industry standard on how you go about selecting load cells for sale. There are also some challenges you may encounter, including finding the compatible load cell amplifier module or signal conditioner or requiring a custom product that would increase the product’s delivery time.

To help you select your sensor, FUTEK developed an easy to follow, 5-Steps guide. Here is a glimpse to help you narrow down your choices. Check out our “Important Considerations in Selecting a force measurement sensor” complete guide for further information.

  • Step 1: Understand your application and what you are measuring. Load sensors are different from pressure sensors or torque sensors and they are designed to measure tension and compression loads.
  • Step 2: Define the sensor mounting characteristics and its assembly. Do you have static load or is it a dynamic type? Define the mounting type. How will you be mounting this Sensor?

 

In-Line Diagram load cell sizing how to select a load cell
In-Line Diagram load cell sizing how to select a load cell
In-Line Diagrams
Side Mount Diagram load cell sizing how to select a load cell

Side Mount Diagram load cell sizing how to select a load cell
Side Mount Diagrams
  • Step 3: Define your minimum and maximum capacity requirements. Be sure to select the capacity over the maximum operating load and determine all extraneous load (side loads or off-center loads) and moments prior to selecting the capacity.
  • Step 4: Define your size and geometry requirements (width, weight, height, length, etc) and mechanical performance requirements (output, nonlinearity, hysteresis, creep, bridge resistance, resolution, frequency response etc.) Other characteristics to consider include waterproof force sensor (aka submersible load cell), cryogenic, high temperature, multiple or redundant bridges, and TEDS IEEE1451.4.
  • Step 5: Define the type of output your application requires. Transducer circuits outputs voltage in mV/V. So, if your PLC or DAQ requires  analog output (i.e. 4-20ma load cell analog output), digital load cell output or serial communication, you will certainly need a load cell amplifier or signal conditioner. Some applications require a handheld display or a load cell indicator for local load cell readout. Make sure to select the right amplifier as well as calibrate the entire measurement system (load transducer + signal conditioner). This turnkey solution translates into more compatibility and accuracy of the entire load measurement system.

When combined with draw wire sensor (aka string potentiometer), load cells are the linchpin of modern factory automation.

For more details on our 5-Steps Guide, please visit our “How to choose a Force Measurement Sensor” for complete guidelines.