Noise is an unwanted additional signal, or distortion of signal, which results in unstable readings. It can occur due to a variety of sources and can have a negative impact on your sensor’s performance. So, how do you avoid this from happening? We created this short guide to help you minimize noise in your force measurement system.
COMMON SOURCES OF ELECTRICAL NOISE
Lights
Generators
Fans
Motors
RF signals
Industrial Machinery
Cell Phones
Computers
Switches and relays
SIGNAL DISTORTED BY NOISE
When testing for noise, it is helpful to test one component first and then add the next component, observing variations in noise as the system is built up. Grounding inputs to components can help determine how much noise that component is contributing or receiving.
Figure 1. Desired Signal
Figure 2. Signal with Noise
TESTING FOR NOISE
1. On the DAQ/PLC or USB and computer system, ground all inputs and observe how much noise is present. This should give you an idea of how much noise your system will generate.
2. Attach the cable for the sensor, or amplifier, to the DAQ/PLC. Then ground the input through the cable to the DAQ/PLC. This will show how much noise the cable adds to the system.
3. Attach the sensor or amplifier to the cable and observe any additional noise. If you’re connecting an amplifier, continue testing noise in the system by grounding the input to the amplifier.
4. Turn on and off equipment nearby to test for sources of noise while observing noise in components.
REDUCING NOISE
Below are some tips on reducing noise. For instruments that have inherent noise, refer to the instrument spec sheet for expected noise levels.
Drawing Number: AP1078