Shop FUTEK
CALL US TODAY
+1 (949) 465-0900
Applications ► Load Cell ► Automotive Pedal Force Testing
 
    By Sensor Type
  • Load Cells
  • Torque Sensors
  • Pressure Sensors
  • Multi-Axis Sensors
    By Industry Type
  • Aerospace & Defense
  • Agricultural
  • Automation
  • Automotive
  • Manufacturing
  • Material & Endurance Testing
  • Medical & Pharmaceutical
  • Product Development & OEM
  • Robotic & System Integrators
    
Application 115

Automotive Pedal Force Testing

  |  
Application Summary
Utilizing FUTEK's Pedal Force Sensors, automotive manufacturers are able to verify the safety and reliability of their automobile's braking mechanics.
Products in Use
Pedal Force Sensor (LAU Series) paired with Instrumentation (IPM650, IHH500, USB Solutions, or IAA Series Amplifiers). View Product Details
Load Cell - Automotive Pedal Force Testing
How it Works
  1. Brake system testing is normally carried out during various stages of the manufacturing process. It starts in the initial development stage, followed by endurance, lab and track testing, and continues through the production process for added quality assurance.
  2. In this particular application, operators may utilize FUTEK's LAU220 Pedal Force Sensor, which is equipped with a mounting plate to ease installation.
  3. Mounted to the top of the automobile's brake pedal, this pedal force sensor accurately measures and records applied forces during scheduled tests. These tests are carried out to validate the integrity of the brake system.
  4. The top surface of the sensor is spherical, centralizing the impact force.
  5. Operators can monitor the data via FUTEK’s IHH500 Intelligent Digital Hand Held Display or IPM650 Panel Mount Display; or it can be streamed to a computer via FUTEK’s USB Solutions.
  6. The data can then be monitored through FUTEK's SENSIT™ Test and Measurement Software. SENSIT™ can monitor up to 16 channels of measurement readings, as well as live graph and data log.
  7. This system can also be utilized for accelerator, clutch, and parking brake pedal testing.
All FUTEK application illustrations are strictly conceptual. Please contact us with questions.
Load Cell - LAU SERIES - Pedal Force Sensors
LAU SERIES
Pedal Force Sensors
Load Cell - IAA Series - Analog Amplifier
IAA Series
Analog Amplifier
Load Cell - USB SOLUTIONS - High Resolution USB Output Module
USB SOLUTIONS
High Resolution USB Output Module
Load Cell - IHH500 - Intelligent Digital Hand Held Display
IHH500
Intelligent Digital Hand Held Display
Load Cell - IPM650 - Panel Mount Display
IPM650
Panel Mount Display
Load Cell - SOFTWARE - SENSIT™ Test and Measurement
SOFTWARE
SENSIT™ Test and Measurement
Subscribe to our e-newsletter!
10 Thomas, Irvine, CA 92618 USA
Tel: (949) 465-0900
Fax: (949) 465-0905


©1998-2018 FUTEK Advanced Sensor Technology, Inc. All rights reserved.

All other trademarks, service marks and logos used in this website are the property of their respective owners.