FUTEK will be closed Thursday, November 23 and Friday, November 24 for the Thanksgiving holiday. We will reopen on Monday, November 27.
Shop FUTEK
CALL US TODAY
+1 (949) 465-0900
Applications ► Torque Sensor ► Torque Sensors for Robot Joint Control
 
    By Sensor Type
  • Load Cells
  • Torque Sensors
  • Pressure Sensors
  • Multi-Axis Sensors
    By Industry Type
  • Aerospace & Defense
  • Agricultural
  • Automation
  • Automotive
  • Manufacturing
  • Material & Endurance Testing
  • Medical & Pharmaceutical
  • Product Development & OEM
  • Robotic & System Integrators
    
Application 316

Torque Sensors for Robot Joint Control

  |  
Application Summary
Versatile and adaptive robotic armatures have the benefit of increasing manufacturing productivity by automating and performing complex, repetitive tasks 24x7. These arms are often designed to be trainable or operate as a team as cooperative robots (cobot/co-robot). Driving these arms in their joints are servo or stepper motors. In addition to monitoring shaft position, these arms need to monitor torque output for smooth, steady motion. By combining these motors with a reaction torque sensor, control loops can be developed for smooth, autonomous operation.
Products in Use
A FUTEK TFF Series Reaction Torque Sensor with Thru Hole Center paired with FUTEK Amplifiers (IAA Series or IDA100). View Product Details
Torque Sensor - Torque Sensors for Robot Joint Control
How it Works
  1. A TFF Series Reaction Torque Sensor is mounted between the robot arm servo motor and it's mounting points.
  2. The torque sensor measures the torque outputted during arm movement which is then amplified by the IAA Series or IDA100 amplifier.
  3. The amplified signal is then sent to the PLC or robotic arm controller, providing precision feedback and closing the control loop.
  4. Additionally, with the IDA100, amplified output from the sensor can be monitored and analog amplifier settings can be adjusted digitally with FUTEK's SENSIT™ Software.
All FUTEK application illustrations are strictly conceptual. Please contact us with questions.
Torque Sensor - TFF Series - Reaction Torque Sensor with Thru Hole Center
TFF Series
Reaction Torque Sensor with Thru Hole Center
Torque Sensor - IAA Series - Analog Amplifiers
IAA Series
Analog Amplifiers
Torque Sensor - IDA100 - Digitally Configurable Amplifier
IDA100
Digitally Configurable Amplifier
Subscribe to our e-newsletter!
10 Thomas, Irvine, CA 92618 USA
Tel: (949) 465-0900
Fax: (949) 465-0905


©1998-2016 FUTEK Advanced Sensor Technology, Inc. All rights reserved.

All other trademarks, service marks and logos used in this website are the property of their respective owners.