Shop FUTEK
CALL US TODAY
+1 (949) 465-0900
 
FUTEK News Room
Futek Developed the Expertise for Million Lb High Capacity Load Cell
Release Date: 11/15/2004
Futek has established its leadership in the Sensor industry for a complete line of very large capacity custom load cells up to 1 million lb. Per customers? requirements, Futek can also provide dead weight calibration of that capacity in tension and compression. The most recent units designed and manufactured at Futek are Q10654 column load cell of 750,000 lb capacity, and Q11065 thru hole low profile load washer of 600,000 lb capacity. The NIST deadweight calibration results of two Q11065 units were found to be 6 times better than printed specs. Enter "102948" and "102949" as sensor ID numbers at Calibration Record Center to access the calibration results.