Torque Transducer, are also commonly known as a Torque Sensor. A Torque Sensor, is a transducer that converts a torsional mechanical input into an electrical output signal.
FUTEK Advanced Sensor Technology’s Torque Transducers, feature both Reaction and Rotary Torque Transducers, in which the former use static and the latter uses dynamic torque mechanics.
Reaction Torque Transducers, utilize a strain gage full bridge configuration that is maintenance free with immovable non-rotating parts that can be used to check residual torque on a fastener. For example, our compact TAT200 Mini Screw Driver Reaction Torque Transducer, may be used to determine the necessary torque involved to resume tightening and thus overcoming frictional effects of a fastener.
FUTEK Rotary Torque Transducers, dynamic torque mechanics offer the best advantage for accurate measurements in power tool performance. We offer non-contact in-line mounting configurations and are capable of sensing torsional rotational speeds up to 12,000 RPM.
From submersible to space, FUTEK Advanced Sensor Technology Torque Transducers, cover an array of applications in many industries ranging from Medical, Automotive, Aviation, Aerospace, Computer, & Automation just to name a few.
FUTEK Advanced Sensor Technology’s industry listing is as broad as its Sensor selection. Our selection of Torque Transducers, can be categorized by the following styles: