Shop FUTEK
CALL US TODAY
+1 (949) 465-0900
Applications ► Pressure Sensor ► Hybrid Rocket Propulsion Pressure Monitoring
 
    By Sensor Type
  • Load Cells
  • Torque Sensors
  • Pressure Sensors
  • Multi-Axis Sensors
    By Industry Type
  • Aerospace & Defense
  • Agricultural
  • Automation
  • Automotive
  • Manufacturing
  • Material & Endurance Testing
  • Medical & Pharmaceutical
  • Product Development & OEM
  • Robotic & System Integrators
    
Application 502

Hybrid Rocket Propulsion Pressure Monitoring

  |  
Application Summary
Pressure monitoring is a critical feature in the design, testing, and operation of Hybrid Rocket Engines. With gaseous or liquid components, rapid pressure spikes in the system can cause catastrophic failure. With monitoring systems in place, complex actions can be taken before failure or activation of pressure relief systems, preserving the system and the mission. Additionally, pressure monitoring can provide feedback on the performance of the system, allowing for system optimization. Typical pressure sensors on the market are limited to a 1kHz natural frequency, whereas the PFT510 series features natural frequencies between 6 kHz and 100 kHz.
Products in Use
FUTEK’s Miniature Flush Mount Pressure Sensor (PFT Series) coupled with high bandwidth, high-frequency instrumentation (IAA300 and USB530) View Product Details
Pressure Sensor - Hybrid Rocket Propulsion Pressure Monitoring
How it Works
  1. A PFT Series pressure sensor is threaded in and mounted flush with the inner walls of the oxidizer tank.
  2. During operation, tank pressure is measured by the pressure sensor.
  3. Output can also be streamed and logged via the USB530 to a PC running SENSIT or connected to a PLC or DAQ with the IAA300.
All FUTEK application illustrations are strictly conceptual. Please contact us with questions.
Pressure Sensor - PFT Series  - Miniature Pressure Sensor – Flush Mount Diaphragm
PFT Series
Miniature Pressure Sensor – Flush Mount Diaphragm
Pressure Sensor - IAA Series - Analog Amplifier
IAA Series
Analog Amplifier
Pressure Sensor - USB530 - External USB Kit (Amplified/Non Amplified + Encoder Input)
USB530
External USB Kit (Amplified/Non Amplified + Encoder Input)
Subscribe to our e-newsletter!
10 Thomas, Irvine, CA 92618 USA
Tel: (949) 465-0900
Fax: (949) 465-0905


©1998-2018 FUTEK Advanced Sensor Technology, Inc. All rights reserved.

All other trademarks, service marks and logos used in this website are the property of their respective owners.