Supportkeyboard_arrow_right

S-Beam Load Cell Applications

 
A Solution for all markets
LSB Series Applications
The LSB Series is specifically designed for In-Line endurance testing; and is versatile enough to fit applications unique, especially in the medical field. Examples of applications utilizing these load cells are industrial automation, medical bag-weighing, and wire tension measurements. The LSB Series fits In-Line applications that require precision measurements, without the anticipation of side loads.
Medical Bag Weighing
Medical applications require the utmost precision. In IV or saline bag weighing, highprecision, In-Line load cells are needed. For this application, FUTEK’s LSB200 Miniature S-Beam Load Cell will measure the tension force applied by an IV bag ...

View Application
Wire Tension Measurement
Wire tension measurement is an integral part for manufacturers of fibers, cables, and even textile fabrics. This method of measurement allows manufactures to ensure their products fit their requirements ...

View Application
Linear Test Stand
Many industries use test fixtures to measure their presses or impact stands. FUTEK’s LSB200 Load Cell is suitable for applications needing precise lower capacity impact test measurements ...

View Application
Multihead Weigher
Load Cells and Force Sensors are commonly used to automate production lines. By using these sensors, production engineers are better able to control the automation process and improve their overall quality ...

View Application
Automation Container Filling
FUTEK’s load cells are designed to fit applications like industrial automation container filling and/or weighing. A load cell is installed in an automation line to help monitor equal distribution through packaging ...

View Application
FUTEK Certifications
Z540-1 ANSI Certified17025 ISO Certified9001 ISO Certified13485 ISO CertifiedU.S. Manufacturer
FUTEK Social Media
Please follow us on linked inPlease follow us on twitterPlease follow us on youtubePlease Email us for additional info
FUTEK Address
10 Thomas, Irvine,
CA 92618 USA
All other trademarks, service marks and logos used in this website are the property of their respective owners.
© 1998–2024 FUTEK Advanced Sensor Technology, Inc. All rights reserved.
Multi Axis Sensor, Force, TorquesBeamLoadCellApplications