Applications keyboard_arrow_right Multi-axis Sensor  |  Quadcopter Propeller Testing

Multi-axis Sensor - Quadcopter Propeller Testing

Professional and hobbyist level quadcopters and drones are becoming more popular in the marketplace. A quadcopter by definition uses its four propellers to generate air lift and change directions. The propellers are designed to work in conjunction with each other to ensure that there are no torque imbalances to send the vehicle spinning out of control.


How it Works
  1. In order to characterize the thrust and torque generated by each motor and propeller, a MBA500 is fixed to the motor's end

  2. When the motor is powered on and rotating, the thrust of the propellers will be measured by the MBA500’s Fz channel, and the back-torque of the motor is measured by the Mz channel, all while maintaining low crosstalk.

  3. This multi-axial sensor, when used with a USB220, allows for a portable setup where a hobbyist/test engineer can use a laptop to analyze the live data of a test both in an outdoor setting or in a more controlled, indoor environment.

Products in Use

MBA500 Torque and Thrust Biaxial Sensor paired with Instrumentation (USB220 and IAA Amplifier).


Contact Us
All FUTEK application illustrations are strictly conceptual.
Please Contact Us with questions.

Professional and hobbyist level quadcopters and drones are becoming more popular in the marketplace. A quadcopter by definition uses its four propellers to generate air lift and change directions. The propellers are designed to work in conjunction with each other to ensure that there are no torque imbalances to send the vehicle spinning out of control.


Quadcopter Propeller Testing
FUTEK Certifications
Z540-1 ANSI Certified17025 ISO Certified9001 ISO Certified13485 ISO CertifiedU.S. Manufacturer
FUTEK Social Media
Please follow us on linked inPlease follow us on twitterPlease follow us on youtubePlease Email us for additional info
FUTEK Address
10 Thomas, Irvine,
CA 92618 USA
All other trademarks, service marks and logos used in this website are the property of their respective owners.
© 1998–2023 FUTEK Advanced Sensor Technology, Inc. All rights reserved.
Multi Axis Sensor, Force, Torqueapplications Quadcopter-Propeller-Testing
+
Z540-1 ANSI Certified17025 ISO Certified9001 ISO Certified13485 ISO CertifiedU.S. Manufacturer
+
Please follow us on linked inPlease follow us on twitterPlease follow us on youtubePlease Email us for additional info
+
10 Thomas, Irvine,
CA 92618 USA
All other trademarks, service marks and logos used in this website are the property of their respective owners.
© 1998–2023 FUTEK Advanced Sensor Technology, Inc. All rights reserved.