Applications keyboard_arrow_right Load Cell  |  Industrial Wire Tension Measurement
Application 124
Industrial Wire Tension Measurement
Application Summary

Wire tension measurement is an integral part for manufacturers of fibers, cables, and even textile fabrics. Industrial cable manufacturers utilize load cells to monitor the tensile forces of their cable.


Products in Use

Miniature Threaded In Line Load Cell (LCM Series) paired with Instrumentation (IAA Series, IPM650, IHH500, USB Solutions).


How it Works
  1. Utilizing FUTEK's LCM Series Miniature Threaded In Line Load Cell coupled with rod end bearings, provides any cable manufacturer with a high-endurance feedback solution.

  2. Due to its compact size, the LCM Series integrates easily into various cable tension applications.

  3. As the operator or manufacturer performs this particular cable tension test, results can then be displayed on various instruments or amplified utilizing an IAA Series Analog Amplifier.

  4. The analog output of the sensor can be taken to either of FUTEK's digital displays - the IHH500 Intelligent Digital Hand Held Display or IPM650 Panel Mount Display - or digitally streamed to FUTEK's USB  Solution.

  5. Pairing any of these instruments with FUTEK’s SENSIT™ Test and Measurement Software allows the collection of all the results.

  6. Note: For outdoor use, protection from the elements is required. FUTEK offers optional encapsulation to protect from moisture.

All FUTEK application illustrations are strictly conceptual. Please Contact Us with questions.
10 Thomas, Irvine, CA 92618 USA
Tel: (949) 465-0900
Fax: (949) 465-0905
© 1998–2019 FUTEK Advanced Sensor Technology, Inc. All rights reserved.
All other trademarks, service marks and logos used in this website are the
property of their respective owners.
certificationscertificationscertificationscertificationscertifications