Loading...

Amplifiers & Signal Conditioners - IDA Series Support | FUTEK

 
Spec Sheets
Resources
Reference Documents
IDA100 FAQ
Is there a separate power supply for the analog output and the USB output portion?
The IDA100 USB communications and analog output are both powered off the same USB2.0 connection.
Does the IDA100 have to be connected to a computer for analog output?
The IDA100 amplified analog output can be used independently from usage with a computer.
How is the IDA100 analog output configured and setup?
The IDA100 analog output is configured and set through the FUTEK SENSITâ„¢ Software or through the FUTEK DLL file.
What is the format of the of the USB readings in SENSIT?
SENSIT displays the same voltage output as the analog output. The Scale Method in SENSIT can be used to change the units into an engineering unit, such as lb.

Application Questions?

FUTEK's Application Engineers are always eager to answer an application question or to simply assist you configure a sensor system that is a fit for you application environment.

Troubleshooting Questions?

Having trouble with your existing sensor or instrumentation? Feel free to contact our technical support experts to assist you.