Applications keyboard_arrow_right Load Cell  |  Medical Patient Lift

Load Cell - Medical Patient Lift

Most medical facilities are equipped with various patient lifting apparatuses. Being that these lifts endure a variety of payloads, load cells are used to monitor the maximum weight capacities.


How it Works
  1. Medical device engineers often utilize robust medical load cell to provide critical verification measurements on patient lifts, being as these lifts support patients of various weights.

  2. Installed on the lift's cable, FUTEK's Pancake Load Cell (LCF Series) measures the weight of load, as well as the endurance of the cable as it maneuvers each patient.

  3. These measurements can be amplified through an IAA Series Analog Amplifier to a PLC, shown on a digital display (IPM650 or IHH500) or streamed directly to a PC using FUTEK's USB Solutions.

  4. If the instrument is paired with FUTEK's SENSIT™ Test and Measurement Software operators can log, and graph all the data on the PC.

Products in Use

A Pancake Load Cell (LCF Series) paired with Instrumentation (IAA Series, IPM650, IHH500, USB Solutions).


Contact Us
All FUTEK application illustrations are strictly conceptual.
Please Contact Us with questions.

Most medical facilities are equipped with various patient lifting apparatuses. Being that these lifts endure a variety of payloads, load cells are used to monitor the maximum weight capacities.


medical load cell
Multi Axis Sensor, Force, Torqueapplications Medical-Patient-Lift
+
Z540-1 ANSI Certified17025 ISO Certified9001 ISO Certified13485 ISO CertifiedU.S. Manufacturer
+
Please follow us on linked inPlease follow us on twitterPlease follow us on youtubePlease Email us for additional info
+
10 Thomas, Irvine,
CA 92618 USA
All other trademarks, service marks and logos used in this website are the property of their respective owners.
© 1998–2023 FUTEK Advanced Sensor Technology, Inc. All rights reserved.