Reaction Torque Sensors are frequently used as auditing tools. This application is utilizing FUTEK’s TDF Torque Sensor to verify the precision of a torque wrench. FUTEK specializes in torque sensor calibration and is equipped with A2LA accredit calibration lab to support critical applications.
Torque Sensor Calibration is an adjustment or set of corrections that are performed on a torque transducer to make sure that the sensor operates as accurately, or error-free, as possible.
One Reaction Torque Sensor (TDF Series) paired with Instrumentation (IPM650, IHH500 or USB Solution) for calibration of torque sensor.
FUTEK’s TDF Series is an efficient torque calibration tool to use when auditing torque wrenches and also for torque transducer calibration.
In this application, the TDF Reaction Torque Sensor is fixed to a mounting plate and coupled to a torque wrench using a male/female adapter.
As the operator ratchets the torque wrench up and down, FUTEK’s TDF Sensor will measure the torque being applied.
These measurements are sent directly to a paired instrument. Depending on instrument selection, the operator can either view the data on a digital display or stream the data directly onto a PC.
If the data shows any anomalies, the torque wrench may be in need of a torque sensor recalibration to meet its intended spec.
Every sensor is prone to measurement errors. These structural uncertainties are the simply algebraic difference between the value that is indicated by the sensor output versus the actual value of the measured variable, or known reference loads. Measurement errors can be caused by many factors:
1) Zero offset (or load cell zero balance)
2) Linearity (or non-linearity)
3) Hysteresis
4) Repeatability (or non-repeatability)
5) Temperature Shift Span and Zero
For more information about torque sensor calibration, visit our Calibration Page.