Supportkeyboard_arrow_right

Torque Sensors

Torque Sensors manufactured in US by FUTEK Advanced Sensor Technology (FUTEK), offering a huge selection of Torque Sensors, utilizing one of the most advanced technologies in the Sensor Industry: Metal foil strain gauge technology.

A Torque Sensor, is a transducer that converts a torsional mechanical input into an electrical output signal. Torque Sensor, are also commonly known as a Torque Transducer.

READ MORE
Metal foil strain gauge based technology facilitates a design of Torque Sensor through the following ‘Lehman’ described process (by department):
  1. A Torque ‘flexure,’ a physical unit comprised of high strength materials, is designed and fabricated by FUTEK Advanced Sensor Technologies Engineering Team and In-House Machine shop, respectively.
  2. Metal foil strain gauges are then bonded to a ‘web’ or most sensitive area of the flexure by FUTEK Advanced Sensor Technology’s Lamination Department.
  3. The Metal foil strain gauge Wheatstone bridge configuration is then wired by our specialized department while accounting for temperature compensation affects of the transducer/sensor.
  4. When Our NIST Traceable Calibration Department applies a mechanical moment, a weight placed upon a moment arm either in the clockwise or counter-clockwise direction, the strain gauge then does its magic by capitalizing in this mechanical deformation and thus producing an electrical resistance change proportional to the load.

FUTEK Advanced Sensor Technology’s Torque Sensors, feature both Reaction and Rotary Torque Sensors, in which the former use static and the latter uses dynamic torque mechanics.

Reaction Torque Sensors, utilize a strain gage full bridge configuration that is maintenance free with immovable non-rotating parts that can be used to check residual torque on a fastener. For example, our compact TAT200 Mini Screw Driver Reaction Torque Sensor, may be used to determine the necessary torque involved to resume tightening and thus overcoming frictional effects of a fastener.

FUTEK Rotary Torque Sensors, dynamic torque mechanics offer the best advantage for accurate measurements in power tool performance. We offer non-contact in-line mounting configurations and are capable of sensing torsional rotational speeds up to 12,000 RPM.

FUTEK Advanced Sensor Technologies strain gauge based torque sensors are widely known in many industries to contain:
  • The Highest accuracy which may conform to many standards from the Automotive to Aerospace.
  • Robust Construction made of either high strength Stainless steel or Aluminum.
  • A guarantee to perform at longest possible work life even at the most rigorous conditions
  • A plethora of mounting options for ANY scale ANY-where.
  • Competitive pricing that separates FUTEK Advanced Sensor Technology from the rest.
  • A full gamut of selections with capacities ranging from 5 in.-oz. to 500,000 in-lbs in both Reaction/Rotary.
  • High Frequency Response coupled with mechanically stiff designs

From submersible to space, FUTEK Advanced Sensor Technology Torque Sensors, cover an array of applications in many industries ranging from Medical, Automotive, Aviation, Aerospace, Computer, & Automation just to name a few.

FUTEK Advanced Sensor Technology’s industry listing is as broad as its Sensor selection. Our selection of Torque Sensors, can be categorized by the following styles:

  • Air Tool Reaction Torque Sensor (Designed as an integral part of nut-runner for automation assembly)
  • Flange to Flange Reaction Torque Sensor (Flange mounted reaction Torque Sensor)
  • Hex Drive Rotary Torque Sensor (Slip ring and non-contact rotary torque measurement for in-line application and available with encoders)
  • Screw driver reaction Torque Sensor (Used in low torque fastener torque auditing assembly).
  • Shaft to Shaft Rotary Torque Sensor (Slip ring and non-contact rotary torque measurement for in-line application and available with encoders)
  • Shaft to Shaft Reaction Torque Sensor (Shaft mounted reaction torque transducers)
  • Socket Extension Reaction Torque Sensor (Widely used in digitizing and verifying applied torque).
  • Square Drive Rotary Torque Sensor (Slip ring and non-contact rotary torque measurement for in-line application, available with encoders)
  • Square Drive to Flange Reaction Torque Sensor (Designed for auditing torque measuring devises and fastener auditing tools)
  • Square Drive to Square Drive Reaction Torque Sensor (Female square drive mounted reaction torque transducers)
  • Torque Wrench Reaction Torque Sensor (Commonly used for fastener torque auditing)
HIDE TEXT
FUTEK Certifications
Z540-1 ANSI Certified17025 ISO Certified9001 ISO Certified13485 ISO CertifiedU.S. Manufacturer
FUTEK Social Media
Please follow us on linked inPlease follow us on twitterPlease follow us on youtubePlease Email us for additional info
FUTEK Address
19 Morgan, Irvine,
CA 92618 USA
All other trademarks, service marks and logos used in this website are the property of their respective owners.
© 1998–2025 FUTEK Advanced Sensor Technology, Inc. All rights reserved.
Multi Axis Sensor, Force, Torquetorque-sensors
+
Z540-1 ANSI Certified17025 ISO Certified9001 ISO Certified13485 ISO CertifiedU.S. Manufacturer
+
Please follow us on linked inPlease follow us on twitterPlease follow us on youtubePlease Email us for additional info
+
19 Morgan, Irvine,
CA 92618 USA
All other trademarks, service marks and logos used in this website are the property of their respective owners.
© 1998–2025 FUTEK Advanced Sensor Technology, Inc. All rights reserved.