Load Cell - Dual Tank Level Controller

Implementing load cells and instrumentation can automate multiple systems within tank dispensing applications. This process ensures operators precision measurements in liquid ratios and triggers for valve opening and closing.


How it Works

  1. In this particular application, specific ratios of each liquid must be dispensed into mixing container prior to its release into each jar.

  2. The selection of load cells can vary from pancake type to donut/thru hole or load button depending on the preferred mounting configuration and required precision. Equally important is the selection of electronics to build this platform.

  3. To ensure that these liquids ratios are exact, several load cells have been installed at the base of each liquid dispensing silo.

  4. Each silo has been paired with either FUTEK’s IHH500 Intelligent Digital Hand Held Display or IPM650 Panel Mount Display. These instruments will monitor the measurements captured by the load

  5. In such setups, electronic options such as output options (analog vs. voltage), alarms/relays, and high resolution measurement can ease installation and improve system readings.

  6. Once a specific ratio of liquid has been released from each silo, the IHH500 or IPM650 will trigger the control valve to close.

  7.  Then the contents in the mixing container can be released into the jar below.

Products in Use

Multiple Pancake Load Cells (LCF Series) paired with Instrumentation (USB Solutions, IHH500 and IPM650). 


Contact Us

All FUTEK application illustrations are strictly conceptual.
Please Contact Us with questions.

Implementing load cells and instrumentation can automate multiple systems within tank dispensing applications. This process ensures operators precision measurements in liquid ratios and triggers for valve opening and closing.